管道
源代码
Python
PythonGitHub
1import depthai as dai
2import cv2
3import numpy as np
4
5def draw_rotated_rectangle(frame, center, size, angle, color, thickness=2):
6 """
7 Draws a rotated rectangle on the given frame.
8
9 Args:
10 frame (numpy.ndarray): The image/frame to draw on.
11 center (tuple): The (x, y) coordinates of the rectangle's center.
12 size (tuple): The (width, height) of the rectangle.
13 angle (float): The rotation angle of the rectangle in degrees (counter-clockwise).
14 color (tuple): The color of the rectangle in BGR format (e.g., (0, 255, 0) for green).
15 thickness (int): The thickness of the rectangle edges. Default is 2.
16 """
17 # Create a rotated rectangle
18 rect = ((center[0], center[1]), (size[0], size[1]), angle)
19
20 # Get the four vertices of the rotated rectangle
21 box = cv2.boxPoints(rect)
22 box = np.intp(box) # Convert to integer coordinates
23
24 # Draw the rectangle on the frame
25 cv2.polylines(frame, [box], isClosed=True, color=color, thickness=thickness)
26
27def processDepthFrame(depthFrame):
28 depth_downscaled = depthFrame[::4]
29 if np.all(depth_downscaled == 0):
30 min_depth = 0
31 else:
32 min_depth = np.percentile(depth_downscaled[depth_downscaled != 0], 1)
33 max_depth = np.percentile(depth_downscaled, 99)
34 depthFrameColor = np.interp(depthFrame, (min_depth, max_depth), (0, 255)).astype(np.uint8)
35 return cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_HOT)
36
37with dai.Pipeline() as pipeline:
38 color = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_A)
39 monoLeft = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_B)
40 monoRight = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_C)
41 stereo = pipeline.create(dai.node.StereoDepth)
42
43 stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.DEFAULT)
44 # stereo.setDepthAlign(dai.CameraBoardSocket.CAM_A)
45 # stereo.setOutputSize(640, 400)
46
47 colorCamOut = color.requestOutput((640, 480))
48
49 monoLeftOut = monoLeft.requestOutput((640, 480))
50 monoRightOut = monoRight.requestOutput((640, 480))
51
52 monoLeftOut.link(stereo.left)
53 monoRightOut.link(stereo.right)
54
55 colorOut = colorCamOut.createOutputQueue()
56 rightOut = monoRightOut.createOutputQueue()
57 stereoOut = stereo.depth.createOutputQueue()
58
59 pipeline.start()
60 while pipeline.isRunning():
61 colorFrame = colorOut.get()
62 stereoFrame = stereoOut.get()
63
64 assert colorFrame.validateTransformations()
65 assert stereoFrame.validateTransformations()
66
67 clr = colorFrame.getCvFrame()
68 depth = processDepthFrame(stereoFrame.getCvFrame())
69
70 rect = dai.RotatedRect(dai.Point2f(300, 200), dai.Size2f(200, 100), 10)
71 remappedRect = colorFrame.getTransformation().remapRectTo(stereoFrame.getTransformation(), rect)
72
73 print(f"Original rect x: {rect.center.x} y: {rect.center.y} width: {rect.size.width} height: {rect.size.height} angle: {rect.angle}")
74 print(f"Remapped rect x: {remappedRect.center.x} y: {remappedRect.center.y} width: {remappedRect.size.width} height: {remappedRect.size.height} angle: {remappedRect.angle}")
75
76 draw_rotated_rectangle(clr, (rect.center.x, rect.center.y), (rect.size.width, rect.size.height), rect.angle, (255, 0, 0))
77 draw_rotated_rectangle(depth, (remappedRect.center.x, remappedRect.center.y), (remappedRect.size.width, remappedRect.size.height), remappedRect.angle, (255, 0, 0))
78
79 cv2.imshow("color", clr)
80 cv2.imshow("depth", depth)
81
82 if cv2.waitKey(1) == ord('q'):
83 break
84 pipeline.stop()需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。