神经辅助立体
Supported on:RVC4

源代码
Python
PythonGitHub
1import numpy as np
2import cv2 as cv
3import depthai as dai
4
5FPS = 20
6
7def showDepth(depthFrame, windowName="Depth", minDistance=500, maxDistance=5000,
8 colormap=cv.COLORMAP_TURBO, useLog=False):
9 """
10 Nicely visualize a depth map.
11
12 Args:
13 depthFrame (np.ndarray): Depth frame (in millimeters).
14 windowName (str): OpenCV window name.
15 minDistance (int): Minimum depth to display (in mm).
16 maxDistance (int): Maximum depth to display (in mm).
17 colormap (int): OpenCV colormap (e.g., cv.COLORMAP_JET, COLORMAP_TURBO, etc.).
18 useLog (bool): Apply logarithmic scaling for better visual contrast.
19
20 Example:
21 frame = depth.getCvFrame()
22 showDepth(frame)
23 """
24 # Convert to float for processing
25 depthFrame = depthFrame.astype(np.float32)
26
27 # Optionally apply log scaling
28 if useLog:
29 depthFrame = np.log(depthFrame + 1)
30
31 # Clip to defined range (avoid far-out values)
32 depthFrame = np.uint8(np.clip(depthFrame, minDistance, maxDistance) / maxDistance * 255)
33
34 # Apply color map
35 depthColor = cv.applyColorMap(depthFrame, colormap)
36
37 # Show in a window
38 cv.imshow(windowName, depthColor)
39
40if __name__ == "__main__":
41 device = dai.Device()
42 pipeline = dai.Pipeline(device)
43 if not device.isNeuralDepthSupported():
44 print("Exiting NeuralAssistedStereo example: device doesn't support NeuralDepth.")
45 exit()
46
47 monoLeft = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_B, sensorFps=FPS)
48 monoRight = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_C, sensorFps=FPS)
49
50 monoLeftOut = monoLeft.requestFullResolutionOutput()
51 monoRightOut = monoRight.requestFullResolutionOutput()
52
53 neuralAssistedStereo = pipeline.create(dai.node.NeuralAssistedStereo).build(monoLeftOut, monoRightOut, neuralModel=dai.DeviceModelZoo.NEURAL_DEPTH_NANO)
54
55 disparityQueue = neuralAssistedStereo.disparity.createOutputQueue()
56
57 with pipeline:
58 pipeline.start()
59 while pipeline.isRunning():
60 disparity = disparityQueue.get()
61 showDepth(disparity.getCvFrame(), minDistance=100, maxDistance=6000, useLog=False)
62
63 key = cv.waitKey(1)
64 if key == ord('q'):
65 quit()需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。