Feature Tracker
Feature Tracker
Demo
Setup
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5from collections import deque
6
7class FeatureTrackerDrawer:
8
9 lineColor = (200, 0, 200)
10 pointColor = (0, 0, 255)
11 circleRadius = 2
12 maxTrackedFeaturesPathLength = 30
13 # for how many frames the feature is tracked
14 trackedFeaturesPathLength = 10
15
16 trackedIDs = None
17 trackedFeaturesPath = None
18
19 def onTrackBar(self, val):
20 FeatureTrackerDrawer.trackedFeaturesPathLength = val
21 pass
22
23 def trackFeaturePath(self, features):
24
25 newTrackedIDs = set()
26 for currentFeature in features:
27 currentID = currentFeature.id
28 newTrackedIDs.add(currentID)
29
30 if currentID not in self.trackedFeaturesPath:
31 self.trackedFeaturesPath[currentID] = deque()
32
33 path = self.trackedFeaturesPath[currentID]
34
35 path.append(currentFeature.position)
36 while(len(path) > max(1, FeatureTrackerDrawer.trackedFeaturesPathLength)):
37 path.popleft()
38
39 self.trackedFeaturesPath[currentID] = path
40
41 featuresToRemove = set()
42 for oldId in self.trackedIDs:
43 if oldId not in newTrackedIDs:
44 featuresToRemove.add(oldId)
45
46 for id in featuresToRemove:
47 self.trackedFeaturesPath.pop(id)
48
49 self.trackedIDs = newTrackedIDs
50
51 def drawFeatures(self, img):
52
53 cv2.setTrackbarPos(self.trackbarName, self.windowName, FeatureTrackerDrawer.trackedFeaturesPathLength)
54
55 for featurePath in self.trackedFeaturesPath.values():
56 path = featurePath
57
58 for j in range(len(path) - 1):
59 src = (int(path[j].x), int(path[j].y))
60 dst = (int(path[j + 1].x), int(path[j + 1].y))
61 cv2.line(img, src, dst, self.lineColor, 1, cv2.LINE_AA, 0)
62 j = len(path) - 1
63 cv2.circle(img, (int(path[j].x), int(path[j].y)), self.circleRadius, self.pointColor, -1, cv2.LINE_AA, 0)
64
65 def __init__(self, trackbarName, windowName):
66 self.trackbarName = trackbarName
67 self.windowName = windowName
68 cv2.namedWindow(windowName)
69 cv2.createTrackbar(trackbarName, windowName, FeatureTrackerDrawer.trackedFeaturesPathLength, FeatureTrackerDrawer.maxTrackedFeaturesPathLength, self.onTrackBar)
70 self.trackedIDs = set()
71 self.trackedFeaturesPath = dict()
72
73
74# Create pipeline
75pipeline = dai.Pipeline()
76
77# Define sources and outputs
78monoLeft = pipeline.create(dai.node.MonoCamera)
79monoRight = pipeline.create(dai.node.MonoCamera)
80featureTrackerLeft = pipeline.create(dai.node.FeatureTracker)
81featureTrackerRight = pipeline.create(dai.node.FeatureTracker)
82
83xoutPassthroughFrameLeft = pipeline.create(dai.node.XLinkOut)
84xoutTrackedFeaturesLeft = pipeline.create(dai.node.XLinkOut)
85xoutPassthroughFrameRight = pipeline.create(dai.node.XLinkOut)
86xoutTrackedFeaturesRight = pipeline.create(dai.node.XLinkOut)
87xinTrackedFeaturesConfig = pipeline.create(dai.node.XLinkIn)
88
89xoutPassthroughFrameLeft.setStreamName("passthroughFrameLeft")
90xoutTrackedFeaturesLeft.setStreamName("trackedFeaturesLeft")
91xoutPassthroughFrameRight.setStreamName("passthroughFrameRight")
92xoutTrackedFeaturesRight.setStreamName("trackedFeaturesRight")
93xinTrackedFeaturesConfig.setStreamName("trackedFeaturesConfig")
94
95# Properties
96monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
97monoLeft.setCamera("left")
98monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
99monoRight.setCamera("right")
100
101# Linking
102monoLeft.out.link(featureTrackerLeft.inputImage)
103featureTrackerLeft.passthroughInputImage.link(xoutPassthroughFrameLeft.input)
104featureTrackerLeft.outputFeatures.link(xoutTrackedFeaturesLeft.input)
105xinTrackedFeaturesConfig.out.link(featureTrackerLeft.inputConfig)
106
107monoRight.out.link(featureTrackerRight.inputImage)
108featureTrackerRight.passthroughInputImage.link(xoutPassthroughFrameRight.input)
109featureTrackerRight.outputFeatures.link(xoutTrackedFeaturesRight.input)
110xinTrackedFeaturesConfig.out.link(featureTrackerRight.inputConfig)
111
112# By default the least mount of resources are allocated
113# increasing it improves performance
114numShaves = 2
115numMemorySlices = 2
116featureTrackerLeft.setHardwareResources(numShaves, numMemorySlices)
117featureTrackerRight.setHardwareResources(numShaves, numMemorySlices)
118
119featureTrackerConfig = featureTrackerRight.initialConfig.get()
120print("Press 's' to switch between Lucas-Kanade optical flow and hardware accelerated motion estimation!")
121
122# Connect to device and start pipeline
123with dai.Device(pipeline) as device:
124
125 # Output queues used to receive the results
126 passthroughImageLeftQueue = device.getOutputQueue("passthroughFrameLeft", 8, False)
127 outputFeaturesLeftQueue = device.getOutputQueue("trackedFeaturesLeft", 8, False)
128 passthroughImageRightQueue = device.getOutputQueue("passthroughFrameRight", 8, False)
129 outputFeaturesRightQueue = device.getOutputQueue("trackedFeaturesRight", 8, False)
130
131 inputFeatureTrackerConfigQueue = device.getInputQueue("trackedFeaturesConfig")
132
133 leftWindowName = "left"
134 leftFeatureDrawer = FeatureTrackerDrawer("Feature tracking duration (frames)", leftWindowName)
135
136 rightWindowName = "right"
137 rightFeatureDrawer = FeatureTrackerDrawer("Feature tracking duration (frames)", rightWindowName)
138
139 while True:
140 inPassthroughFrameLeft = passthroughImageLeftQueue.get()
141 passthroughFrameLeft = inPassthroughFrameLeft.getFrame()
142 leftFrame = cv2.cvtColor(passthroughFrameLeft, cv2.COLOR_GRAY2BGR)
143
144 inPassthroughFrameRight = passthroughImageRightQueue.get()
145 passthroughFrameRight = inPassthroughFrameRight.getFrame()
146 rightFrame = cv2.cvtColor(passthroughFrameRight, cv2.COLOR_GRAY2BGR)
147
148 trackedFeaturesLeft = outputFeaturesLeftQueue.get().trackedFeatures
149 leftFeatureDrawer.trackFeaturePath(trackedFeaturesLeft)
150 leftFeatureDrawer.drawFeatures(leftFrame)
151
152 trackedFeaturesRight = outputFeaturesRightQueue.get().trackedFeatures
153 rightFeatureDrawer.trackFeaturePath(trackedFeaturesRight)
154 rightFeatureDrawer.drawFeatures(rightFrame)
155
156 # Show the frame
157 cv2.imshow(leftWindowName, leftFrame)
158 cv2.imshow(rightWindowName, rightFrame)
159
160 key = cv2.waitKey(1)
161 if key == ord('q'):
162 break
163 elif key == ord('s'):
164 if featureTrackerConfig.motionEstimator.type == dai.FeatureTrackerConfig.MotionEstimator.Type.LUCAS_KANADE_OPTICAL_FLOW:
165 featureTrackerConfig.motionEstimator.type = dai.FeatureTrackerConfig.MotionEstimator.Type.HW_MOTION_ESTIMATION
166 print("Switching to hardware accelerated motion estimation")
167 else:
168 featureTrackerConfig.motionEstimator.type = dai.FeatureTrackerConfig.MotionEstimator.Type.LUCAS_KANADE_OPTICAL_FLOW
169 print("Switching to Lucas-Kanade optical flow")
170
171 cfg = dai.FeatureTrackerConfig()
172 cfg.set(featureTrackerConfig)
173 inputFeatureTrackerConfigQueue.send(cfg)Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.