System information
Demo
Command Line
1Ddr used / total - 0.13 / 414.80 MiB
2 Cmx used / total - 2.24 / 2.50 MiB
3 LeonCss heap used / total - 4.17 / 46.41 MiB
4 LeonMss heap used / total - 2.87 / 27.58 MiB
5 Chip temperature - average: 38.59, css: 39.81, mss: 37.71, upa: 38.65, dss: 38.18
6 Cpu usage - Leon CSS: 7.08%, Leon MSS: 1.48 %
7 ----------------------------------------
8 Ddr used / total - 0.13 / 414.80 MiB
9 Cmx used / total - 2.24 / 2.50 MiB
10 LeonCss heap used / total - 4.17 / 46.41 MiB
11 LeonMss heap used / total - 2.87 / 27.58 MiB
12 Chip temperature - average: 38.59, css: 39.58, mss: 37.94, upa: 38.18, dss: 38.65
13 Cpu usage - Leon CSS: 1.55%, Leon MSS: 0.30 %
14 ----------------------------------------
15 Ddr used / total - 0.13 / 414.80 MiB
16 Cmx used / total - 2.24 / 2.50 MiB
17 LeonCss heap used / total - 4.17 / 46.41 MiB
18 LeonMss heap used / total - 2.87 / 27.58 MiB
19 Chip temperature - average: 38.94, css: 40.04, mss: 38.18, upa: 39.35, dss: 38.18
20 Cpu usage - Leon CSS: 0.56%, Leon MSS: 0.06 %
21 ----------------------------------------
22 Ddr used / total - 0.13 / 414.80 MiB
23 Cmx used / total - 2.24 / 2.50 MiB
24 LeonCss heap used / total - 4.17 / 46.41 MiB
25 LeonMss heap used / total - 2.87 / 27.58 MiB
26 Chip temperature - average: 39.46, css: 40.28, mss: 38.88, upa: 39.81, dss: 38.88
27 Cpu usage - Leon CSS: 0.51%, Leon MSS: 0.06 %
28 ----------------------------------------uparepresents the temperature of the SHAVE blockdssrepresents the temperature of the DDR subsystem
Setup
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5
6def printSystemInformation(info):
7 m = 1024 * 1024 # MiB
8 print(f"Ddr used / total - {info.ddrMemoryUsage.used / m:.2f} / {info.ddrMemoryUsage.total / m:.2f} MiB")
9 print(f"Cmx used / total - {info.cmxMemoryUsage.used / m:.2f} / {info.cmxMemoryUsage.total / m:.2f} MiB")
10 print(f"LeonCss heap used / total - {info.leonCssMemoryUsage.used / m:.2f} / {info.leonCssMemoryUsage.total / m:.2f} MiB")
11 print(f"LeonMss heap used / total - {info.leonMssMemoryUsage.used / m:.2f} / {info.leonMssMemoryUsage.total / m:.2f} MiB")
12 t = info.chipTemperature
13 print(f"Chip temperature - average: {t.average:.2f}, css: {t.css:.2f}, mss: {t.mss:.2f}, upa: {t.upa:.2f}, dss: {t.dss:.2f}")
14 print(f"Cpu usage - Leon CSS: {info.leonCssCpuUsage.average * 100:.2f}%, Leon MSS: {info.leonMssCpuUsage.average * 100:.2f} %")
15 print("----------------------------------------")
16
17# Create pipeline
18pipeline = dai.Pipeline()
19
20# Define source and output
21sysLog = pipeline.create(dai.node.SystemLogger)
22linkOut = pipeline.create(dai.node.XLinkOut)
23
24linkOut.setStreamName("sysinfo")
25
26# Properties
27sysLog.setRate(1) # 1 Hz
28
29# Linking
30sysLog.out.link(linkOut.input)
31
32# Connect to device and start pipeline
33with dai.Device(pipeline) as device:
34
35 # Output queue will be used to get the system info
36 qSysInfo = device.getOutputQueue(name="sysinfo", maxSize=4, blocking=False)
37
38 while True:
39 sysInfo = qSysInfo.get() # Blocking call, will wait until a new data has arrived
40 printSystemInformation(sysInfo)Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.