RGB & Tiny YOLO
This example shows how to run YOLO on the RGB input frame, and how to display both the RGB preview and the metadata results from the YOLO model on the preview. Decoding is done on the RVC instead on the host computer.Configurable, network dependent parameters are required for correct decoding:setNumClasses()- number of YOLO classessetCoordinateSize()- size of coordinatesetAnchors()- yolo anchorssetAnchorMasks()- anchorMasks26, anchorMasks13 (anchorMasks52 - additionally for full YOLOv4)setIouThreshold()- intersection over union thresholdsetConfidenceThreshold()- confidence threshold above which objects are detected
yolo3 as a CMD argument to use Tiny YOLOv3.Demo
Setup
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the scriptCommand Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3"""
4The code is the same as for Tiny Yolo V3 and V4, the only difference is the blob file
5- Tiny YOLOv3: https://github.com/david8862/keras-YOLOv3-model-set
6- Tiny YOLOv4: https://github.com/TNTWEN/OpenVINO-YOLOV4
7"""
8
9from pathlib import Path
10import sys
11import cv2
12import depthai as dai
13import numpy as np
14import time
15
16# Get argument first
17nnPath = str((Path(__file__).parent / Path('../models/yolo-v4-tiny-tf_openvino_2021.4_6shave.blob')).resolve().absolute())
18if 1 < len(sys.argv):
19 arg = sys.argv[1]
20 if arg == "yolo3":
21 nnPath = str((Path(__file__).parent / Path('../models/yolo-v3-tiny-tf_openvino_2021.4_6shave.blob')).resolve().absolute())
22 elif arg == "yolo4":
23 nnPath = str((Path(__file__).parent / Path('../models/yolo-v4-tiny-tf_openvino_2021.4_6shave.blob')).resolve().absolute())
24 else:
25 nnPath = arg
26else:
27 print("Using Tiny YoloV4 model. If you wish to use Tiny YOLOv3, call 'tiny_yolo.py yolo3'")
28
29if not Path(nnPath).exists():
30 import sys
31 raise FileNotFoundError(f'Required file/s not found, please run "{sys.executable} install_requirements.py"')
32
33# tiny yolo v4 label texts
34labelMap = [
35 "person", "bicycle", "car", "motorbike", "aeroplane", "bus", "train",
36 "truck", "boat", "traffic light", "fire hydrant", "stop sign", "parking meter", "bench",
37 "bird", "cat", "dog", "horse", "sheep", "cow", "elephant",
38 "bear", "zebra", "giraffe", "backpack", "umbrella", "handbag", "tie",
39 "suitcase", "frisbee", "skis", "snowboard", "sports ball", "kite", "baseball bat",
40 "baseball glove", "skateboard", "surfboard", "tennis racket", "bottle", "wine glass", "cup",
41 "fork", "knife", "spoon", "bowl", "banana", "apple", "sandwich",
42 "orange", "broccoli", "carrot", "hot dog", "pizza", "donut", "cake",
43 "chair", "sofa", "pottedplant", "bed", "diningtable", "toilet", "tvmonitor",
44 "laptop", "mouse", "remote", "keyboard", "cell phone", "microwave", "oven",
45 "toaster", "sink", "refrigerator", "book", "clock", "vase", "scissors",
46 "teddy bear", "hair drier", "toothbrush"
47]
48
49syncNN = True
50
51# Create pipeline
52pipeline = dai.Pipeline()
53
54# Define sources and outputs
55camRgb = pipeline.create(dai.node.ColorCamera)
56detectionNetwork = pipeline.create(dai.node.YoloDetectionNetwork)
57xoutRgb = pipeline.create(dai.node.XLinkOut)
58nnOut = pipeline.create(dai.node.XLinkOut)
59
60xoutRgb.setStreamName("rgb")
61nnOut.setStreamName("nn")
62
63# Properties
64camRgb.setPreviewSize(416, 416)
65camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
66camRgb.setInterleaved(False)
67camRgb.setColorOrder(dai.ColorCameraProperties.ColorOrder.BGR)
68camRgb.setFps(40)
69
70# Network specific settings
71detectionNetwork.setConfidenceThreshold(0.5)
72detectionNetwork.setNumClasses(80)
73detectionNetwork.setCoordinateSize(4)
74detectionNetwork.setAnchors([10, 14, 23, 27, 37, 58, 81, 82, 135, 169, 344, 319])
75detectionNetwork.setAnchorMasks({"side26": [1, 2, 3], "side13": [3, 4, 5]})
76detectionNetwork.setIouThreshold(0.5)
77detectionNetwork.setBlobPath(nnPath)
78detectionNetwork.setNumInferenceThreads(2)
79detectionNetwork.input.setBlocking(False)
80
81# Linking
82camRgb.preview.link(detectionNetwork.input)
83if syncNN:
84 detectionNetwork.passthrough.link(xoutRgb.input)
85else:
86 camRgb.preview.link(xoutRgb.input)
87
88detectionNetwork.out.link(nnOut.input)
89
90# Connect to device and start pipeline
91with dai.Device(pipeline) as device:
92
93 # Output queues will be used to get the rgb frames and nn data from the outputs defined above
94 qRgb = device.getOutputQueue(name="rgb", maxSize=4, blocking=False)
95 qDet = device.getOutputQueue(name="nn", maxSize=4, blocking=False)
96
97 frame = None
98 detections = []
99 startTime = time.monotonic()
100 counter = 0
101 color2 = (255, 255, 255)
102
103 # nn data, being the bounding box locations, are in <0..1> range - they need to be normalized with frame width/height
104 def frameNorm(frame, bbox):
105 normVals = np.full(len(bbox), frame.shape[0])
106 normVals[::2] = frame.shape[1]
107 return (np.clip(np.array(bbox), 0, 1) * normVals).astype(int)
108
109 def displayFrame(name, frame):
110 color = (255, 0, 0)
111 for detection in detections:
112 bbox = frameNorm(frame, (detection.xmin, detection.ymin, detection.xmax, detection.ymax))
113 cv2.putText(frame, labelMap[detection.label], (bbox[0] + 10, bbox[1] + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
114 cv2.putText(frame, f"{int(detection.confidence * 100)}%", (bbox[0] + 10, bbox[1] + 40), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
115 cv2.rectangle(frame, (bbox[0], bbox[1]), (bbox[2], bbox[3]), color, 2)
116 # Show the frame
117 cv2.imshow(name, frame)
118
119 while True:
120 if syncNN:
121 inRgb = qRgb.get()
122 inDet = qDet.get()
123 else:
124 inRgb = qRgb.tryGet()
125 inDet = qDet.tryGet()
126
127 if inRgb is not None:
128 frame = inRgb.getCvFrame()
129 cv2.putText(frame, "NN fps: {:.2f}".format(counter / (time.monotonic() - startTime)),
130 (2, frame.shape[0] - 4), cv2.FONT_HERSHEY_TRIPLEX, 0.4, color2)
131
132 if inDet is not None:
133 detections = inDet.detections
134 counter += 1
135
136 if frame is not None:
137 displayFrame("rgb", frame)
138
139 if cv2.waitKey(1) == ord('q'):
140 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.