POE set IP
Make sure to set mask and gateway correctly!If they are set incorrectly you will soft-brick your device (you won't be able to access it), and will have to factory reset your OAK PoE.
We suggest using Device Manager, a GUI tool for interfacing with the bootloader and its configurations.
Demo
Command Line
1Found device with name: 192.168.1.136
2 -------------------------------------
3 "1" to set a static IPv4 address
4 "2" to set a dynamic IPv4 address
5 "3" to clear the config
6 1
7 -------------------------------------
8 Enter IPv4: 192.168.1.200
9 Enter IPv4 Mask: 255.255.255.0
10 Enter IPv4 Gateway: 192.168.1.1
11 Flashing static IPv4 192.168.1.200, mask 255.255.255.0, gateway 192.168.1.1 to the POE device. Enter 'y' to confirm. y
12 Flashing successful.Command Line
1Found device with name: 192.168.1.200
2 -------------------------------------
3 "1" to set a static IPv4 address
4 "2" to set a dynamic IPv4 address
5 "3" to clear the configdefault IP address, which it will revert to if no DHCP server is detected. For more details on how this works, please refer to the No DHCP section in the Poe Deployment Guide.Setup
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
C++
Python
PythonGitHub
1import depthai as dai
2
3(found, info) = dai.DeviceBootloader.getFirstAvailableDevice()
4
5def check_str(s: str):
6 spl = s.split(".")
7 if len(spl) != 4:
8 raise ValueError(f"Entered value {s} doesn't contain 3 dots. Value has to be in the following format: '255.255.255.255'")
9 for num in spl:
10 if 255 < int(num):
11 raise ValueError("Entered values can't be above 255!")
12 return s
13
14if found:
15 print(f'Found device with name: {info.name}')
16 print('-------------------------------------')
17 print('"1" to set a static IPv4 address')
18 print('"2" to set a dynamic IPv4 address')
19 print('"3" to clear the config')
20 key = input('Enter the number: ').strip()
21 print('-------------------------------------')
22 if int(key) < 1 or 3 < int(key):
23 raise ValueError("Entered value should either be '1', '2' or '3'!")
24
25 with dai.DeviceBootloader(info) as bl:
26 if key in ['1', '2']:
27 ipv4 = check_str(input("Enter IPv4: ").strip())
28 mask = check_str(input("Enter IPv4 Mask: ").strip())
29 gateway = check_str(input("Enter IPv4 Gateway: ").strip())
30 mode = 'static' if key == '1' else 'dynamic'
31 val = input(f"Flashing {mode} IPv4 {ipv4}, mask {mask}, gateway {gateway} to the POE device. Enter 'y' to confirm. ").strip()
32 if val != 'y':
33 raise Exception("Flashing aborted.")
34
35 conf = dai.DeviceBootloader.Config()
36 if key == '1': conf.setStaticIPv4(ipv4, mask, gateway)
37 elif key == '2': conf.setDynamicIPv4(ipv4, mask, gateway)
38 (success, error) = bl.flashConfig(conf)
39 elif key == '3':
40 (success, error) = bl.flashConfigClear()
41
42 if not success:
43 print(f"Flashing failed: {error}")
44 else:
45 print(f"Flashing successful.")Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.