Calibration Flash

This example shows how to flash calibration data of version 6 (gen2 calibration data) to the device.

Similiar samples:

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script

git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py

For additional information, please follow installation guide

Source code

Also available on GitHub

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
#!/usr/bin/env python3

from pathlib import Path
import cv2
import depthai as dai
import argparse

calibJsonFile = str((Path(__file__).parent / Path('models/depthai_calib.json')).resolve().absolute())
calibBackUpFile = str((Path(__file__).parent / Path('depthai_calib_backup.json')).resolve().absolute())

parser = argparse.ArgumentParser()
parser.add_argument('calibJsonFile', nargs='?', help="Path to V6 calibration file in json", default=calibJsonFile)
args = parser.parse_args()

# Connect device
with dai.Device() as device:

    deviceCalib = device.readCalibration()
    deviceCalib.eepromToJsonFile(calibBackUpFile)
    print("Calibration Data on the device is backed up at:")
    print(calibBackUpFile)
    calibData = dai.CalibrationHandler(args.calibJsonFile)

    status = device.flashCalibration(calibData)
    if status:
        print('Calibration Flash Successful')
    else:
        print('Calibration Flash Failed!!!')

Also available on GitHub

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
#include <cstdio>
#include <filesystem>
#include <iostream>
#include <string>

// Inludes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

int main(int argc, char** argv) {
    std::string calibJsonFile(CALIB_PATH);
    std::string calibBackUpFile("depthai_calib_backup.json");
    if(argc > 1) {
        calibJsonFile = std::string(argv[1]);
    }

    // Connect device
    dai::Device device;

    dai::CalibrationHandler deviceCalib = device.readCalibration();
    deviceCalib.eepromToJsonFile(calibBackUpFile);
    std::cout << "Calibration Data on the device is backed up at:" << calibBackUpFile << std::endl;
    dai::CalibrationHandler calibData(calibJsonFile);

    if(device.flashCalibration(calibData)) {
        std::cout << "Calibration Flash Successful" << std::endl;
    } else {
        std::cout << "Calibration Flash Failed!!!" << std::endl;
    }

    return 0;
}

Got questions?

We’re always happy to help with code or other questions you might have.