DepthAI v2 has been superseded by DepthAI v3. You are viewing legacy documentation.
DepthAI Tutorials
DepthAI API References

ON THIS PAGE

  • RGB Encoding & MobilenetSSD
  • Similar samples:
  • Demo
  • Setup
  • Source code
  • Pipeline

RGB Encoding & MobilenetSSD

This example shows how to configure the depthai video encoder in h.265 format to encode the RGB camera input at Full-HD resolution at 30FPS, and transfers the encoded video over XLINK to the host, saving it to disk as a video file. In the same time, a MobileNetv2SSD network is ran on the frames from the same RGB camera that is used for encodingPressing Ctrl+C will stop the recording and then convert it using ffmpeg into an mp4 to make it playable. Note that ffmpeg will need to be installed and runnable for the conversion to mp4 to succeed.Be careful, this example saves encoded video to your host storage. So if you leave it running, you could fill up your storage on your host.It's a combination of RGB Encoding and RGB & MobilenetSSD.

Similar samples:

Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.py
For additional information, please follow the installation guide.

Source code

Python
C++

Python

Python
GitHub
1#!/usr/bin/env python3
2
3from pathlib import Path
4import sys
5import cv2
6import depthai as dai
7import numpy as np
8
9# Get argument first
10nnPath = str((Path(__file__).parent / Path('../models/mobilenet-ssd_openvino_2021.4_6shave.blob')).resolve().absolute())
11if len(sys.argv) > 1:
12    nnPath = sys.argv[1]
13
14if not Path(nnPath).exists():
15    import sys
16    raise FileNotFoundError(f'Required file/s not found, please run "{sys.executable} install_requirements.py"')
17
18# MobilenetSSD label texts
19labelMap = ["background", "aeroplane", "bicycle", "bird", "boat", "bottle", "bus", "car", "cat", "chair", "cow",
20            "diningtable", "dog", "horse", "motorbike", "person", "pottedplant", "sheep", "sofa", "train", "tvmonitor"]
21
22# Create pipeline
23pipeline = dai.Pipeline()
24
25# Define sources and outputs
26camRgb = pipeline.create(dai.node.ColorCamera)
27videoEncoder = pipeline.create(dai.node.VideoEncoder)
28nn = pipeline.create(dai.node.MobileNetDetectionNetwork)
29
30xoutRgb = pipeline.create(dai.node.XLinkOut)
31videoOut = pipeline.create(dai.node.XLinkOut)
32nnOut = pipeline.create(dai.node.XLinkOut)
33
34xoutRgb.setStreamName("rgb")
35videoOut.setStreamName("h265")
36nnOut.setStreamName("nn")
37
38# Properties
39camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
40camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
41camRgb.setPreviewSize(300, 300)
42camRgb.setInterleaved(False)
43
44videoEncoder.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H265_MAIN)
45
46nn.setConfidenceThreshold(0.5)
47nn.setBlobPath(nnPath)
48nn.setNumInferenceThreads(2)
49nn.input.setBlocking(False)
50
51# Linking
52camRgb.video.link(videoEncoder.input)
53camRgb.preview.link(xoutRgb.input)
54camRgb.preview.link(nn.input)
55videoEncoder.bitstream.link(videoOut.input)
56nn.out.link(nnOut.input)
57
58# Connect to device and start pipeline
59with dai.Device(pipeline) as device, open('video.h265', 'wb') as videoFile:
60
61    # Queues
62    queue_size = 8
63    qRgb = device.getOutputQueue("rgb", queue_size)
64    qDet = device.getOutputQueue("nn", queue_size)
65    qRgbEnc = device.getOutputQueue('h265', maxSize=30, blocking=True)
66
67    frame = None
68    detections = []
69
70    def frameNorm(frame, bbox):
71        normVals = np.full(len(bbox), frame.shape[0])
72        normVals[::2] = frame.shape[1]
73        return (np.clip(np.array(bbox), 0, 1) * normVals).astype(int)
74
75    def displayFrame(name, frame):
76        color = (255, 0, 0)
77        for detection in detections:
78            bbox = frameNorm(frame, (detection.xmin, detection.ymin, detection.xmax, detection.ymax))
79            cv2.putText(frame, labelMap[detection.label], (bbox[0] + 10, bbox[1] + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color)
80            cv2.putText(frame, f"{int(detection.confidence * 100)}%", (bbox[0] + 10, bbox[1] + 40), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color)
81            cv2.rectangle(frame, (bbox[0], bbox[1]), (bbox[2], bbox[3]), color, 2)
82        # Show the frame
83        cv2.imshow(name, frame)
84
85    while True:
86        inRgb = qRgb.tryGet()
87        inDet = qDet.tryGet()
88
89        while qRgbEnc.has():
90            qRgbEnc.get().getData().tofile(videoFile)
91
92        if inRgb is not None:
93            frame = inRgb.getCvFrame()
94
95        if inDet is not None:
96            detections = inDet.detections
97
98        if frame is not None:
99            displayFrame("rgb", frame)
100
101        if cv2.waitKey(1) == ord('q'):
102            break
103
104print("To view the encoded data, convert the stream file (.h265) into a video file (.mp4), using a command below:")
105print("ffmpeg -framerate 30 -i video.h265 -c copy video.mp4")

Pipeline

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.