Mono Camera Control

This example shows how to control the device-side crop and camera triggers. TWo output is a displayed mono cropped frame, that can be manipulated using the following keys:

  1. w will move the crop up

  2. a will move the crop left

  3. s will move the crop down

  4. d will move the crop right

  5. e will trigger autoexposure

  6. i and o will decrease/increase the exposure time

  7. k and l will decrease/increase the sensitivity iso

Similiar samples:

Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script

git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py

For additional information, please follow installation guide

Source code

Also available on GitHub

  1
  2
  3
  4
  5
  6
  7
  8
  9
 10
 11
 12
 13
 14
 15
 16
 17
 18
 19
 20
 21
 22
 23
 24
 25
 26
 27
 28
 29
 30
 31
 32
 33
 34
 35
 36
 37
 38
 39
 40
 41
 42
 43
 44
 45
 46
 47
 48
 49
 50
 51
 52
 53
 54
 55
 56
 57
 58
 59
 60
 61
 62
 63
 64
 65
 66
 67
 68
 69
 70
 71
 72
 73
 74
 75
 76
 77
 78
 79
 80
 81
 82
 83
 84
 85
 86
 87
 88
 89
 90
 91
 92
 93
 94
 95
 96
 97
 98
 99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
#!/usr/bin/env python3

"""
This example shows usage of mono camera in crop mode with the possibility to move the crop.
Uses 'WASD' controls to move the crop window, 'T' to trigger autofocus, 'IOKL,.' for manual exposure/focus:
  Control:      key[dec/inc]  min..max
  exposure time:     I   O      1..33000 [us]
  sensitivity iso:   K   L    100..1600
To go back to auto controls:
  'E' - autoexposure
"""

import cv2
import depthai as dai

# Step size ('W','A','S','D' controls)
stepSize = 0.02
# Manual exposure/focus set step
expStep = 500  # us
isoStep = 50

def clamp(num, v0, v1):
    return max(v0, min(num, v1))

sendCamConfig = False

# Create pipeline
pipeline = dai.Pipeline()

# Define sources and outputs
monoRight = pipeline.createMonoCamera()
monoLeft = pipeline.createMonoCamera()
manipRight = pipeline.createImageManip()
manipLeft = pipeline.createImageManip()

controlIn = pipeline.createXLinkIn()
configIn = pipeline.createXLinkIn()
manipOutRight = pipeline.createXLinkOut()
manipOutLeft = pipeline.createXLinkOut()

controlIn.setStreamName('control')
configIn.setStreamName('config')
manipOutRight.setStreamName("right")
manipOutLeft.setStreamName("left")

# Crop range
topLeft = dai.Point2f(0.2, 0.2)
bottomRight = dai.Point2f(0.8, 0.8)

# Properties
monoRight.setBoardSocket(dai.CameraBoardSocket.RIGHT)
monoLeft.setBoardSocket(dai.CameraBoardSocket.LEFT)
monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
manipRight.initialConfig.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
manipLeft.initialConfig.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
manipRight.setMaxOutputFrameSize(monoRight.getResolutionHeight()*monoRight.getResolutionWidth()*3)

# Linking
monoRight.out.link(manipRight.inputImage)
monoLeft.out.link(manipLeft.inputImage)
controlIn.out.link(monoRight.inputControl)
controlIn.out.link(monoLeft.inputControl)
configIn.out.link(manipRight.inputConfig)
configIn.out.link(manipLeft.inputConfig)
manipRight.out.link(manipOutRight.input)
manipLeft.out.link(manipOutLeft.input)

# Connect to device and start pipeline
with dai.Device(pipeline) as device:

    # Output queues will be used to get the grayscale frames
    qRight = device.getOutputQueue(manipOutRight.getStreamName(), maxSize=4, blocking=False)
    qLeft = device.getOutputQueue(manipOutLeft.getStreamName(), maxSize=4, blocking=False)
    configQueue = device.getInputQueue(configIn.getStreamName())
    controlQueue = device.getInputQueue(controlIn.getStreamName())

    # Defaults and limits for manual focus/exposure controls
    expTime = 20000
    expMin = 1
    expMax = 33000

    sensIso = 800
    sensMin = 100
    sensMax = 1600

    while True:
        inRight = qRight.get()
        inLeft = qLeft.get()
        cv2.imshow("right", inRight.getCvFrame())
        cv2.imshow("left", inLeft.getCvFrame())

        # Update screen (1ms pooling rate)
        key = cv2.waitKey(1)
        if key == ord('q'):
            break
        elif key == ord('e'):
            print("Autoexposure enable")
            ctrl = dai.CameraControl()
            ctrl.setAutoExposureEnable()
            controlQueue.send(ctrl)
        elif key in [ord('i'), ord('o'), ord('k'), ord('l')]:
            if key == ord('i'): expTime -= expStep
            if key == ord('o'): expTime += expStep
            if key == ord('k'): sensIso -= isoStep
            if key == ord('l'): sensIso += isoStep
            expTime = clamp(expTime, expMin, expMax)
            sensIso = clamp(sensIso, sensMin, sensMax)
            print("Setting manual exposure, time:", expTime, "iso:", sensIso)
            ctrl = dai.CameraControl()
            ctrl.setManualExposure(expTime, sensIso)
            controlQueue.send(ctrl)
        elif key == ord('w'):
            if topLeft.y - stepSize >= 0:
                topLeft.y -= stepSize
                bottomRight.y -= stepSize
                sendCamConfig = True
        elif key == ord('a'):
            if topLeft.x - stepSize >= 0:
                topLeft.x -= stepSize
                bottomRight.x -= stepSize
                sendCamConfig = True
        elif key == ord('s'):
            if bottomRight.y + stepSize <= 1:
                topLeft.y += stepSize
                bottomRight.y += stepSize
                sendCamConfig = True
        elif key == ord('d'):
            if bottomRight.x + stepSize <= 1:
                topLeft.x += stepSize
                bottomRight.x += stepSize
                sendCamConfig = True

        # Send new config to camera
        if sendCamConfig:
            cfg = dai.ImageManipConfig()
            cfg.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
            configQueue.send(cfg)
            sendCamConfig = False

Also available on GitHub

  1
  2
  3
  4
  5
  6
  7
  8
  9
 10
 11
 12
 13
 14
 15
 16
 17
 18
 19
 20
 21
 22
 23
 24
 25
 26
 27
 28
 29
 30
 31
 32
 33
 34
 35
 36
 37
 38
 39
 40
 41
 42
 43
 44
 45
 46
 47
 48
 49
 50
 51
 52
 53
 54
 55
 56
 57
 58
 59
 60
 61
 62
 63
 64
 65
 66
 67
 68
 69
 70
 71
 72
 73
 74
 75
 76
 77
 78
 79
 80
 81
 82
 83
 84
 85
 86
 87
 88
 89
 90
 91
 92
 93
 94
 95
 96
 97
 98
 99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
/**
 * This example shows usage of mono camera in crop mode with the possibility to move the crop.
 * Uses 'WASD' controls to move the crop window, 'T' to trigger autofocus, 'IOKL,.' for manual exposure/focus:
 *   Control:      key[dec/inc]  min..max
 *   exposure time:     I   O      1..33000 [us]
 *   sensitivity iso:   K   L    100..1600
 * To go back to auto controls:
 *   'E' - autoexposure
 */
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

// Step size ('W','A','S','D' controls)
static constexpr float stepSize = 0.02;

// Manual exposure/focus set step
static constexpr int EXP_STEP = 500;  // us
static constexpr int ISO_STEP = 50;

static int clamp(int num, int v0, int v1) {
    return std::max(v0, std::min(num, v1));
}

static std::atomic<bool> sendCamConfig{false};

int main() {
    // Create pipeline
    dai::Pipeline pipeline;

    // Define sources and outputs
    auto monoRight = pipeline.create<dai::node::MonoCamera>();
    auto monoLeft = pipeline.create<dai::node::MonoCamera>();
    auto manipRight = pipeline.create<dai::node::ImageManip>();
    auto manipLeft = pipeline.create<dai::node::ImageManip>();

    auto controlIn = pipeline.create<dai::node::XLinkIn>();
    auto configIn = pipeline.create<dai::node::XLinkIn>();
    auto manipOutRight = pipeline.create<dai::node::XLinkOut>();
    auto manipOutLeft = pipeline.create<dai::node::XLinkOut>();

    controlIn->setStreamName("control");
    configIn->setStreamName("config");
    manipOutRight->setStreamName("right");
    manipOutLeft->setStreamName("left");

    // Crop range
    dai::Point2f topLeft(0.2, 0.2);
    dai::Point2f bottomRight(0.8, 0.8);

    // Properties
    monoRight->setBoardSocket(dai::CameraBoardSocket::RIGHT);
    monoLeft->setBoardSocket(dai::CameraBoardSocket::LEFT);
    monoRight->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
    monoLeft->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
    manipRight->initialConfig.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y);
    manipLeft->initialConfig.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y);

    // Linking
    monoRight->out.link(manipRight->inputImage);
    monoLeft->out.link(manipLeft->inputImage);
    controlIn->out.link(monoRight->inputControl);
    controlIn->out.link(monoLeft->inputControl);
    configIn->out.link(manipRight->inputConfig);
    configIn->out.link(manipLeft->inputConfig);
    manipRight->out.link(manipOutRight->input);
    manipLeft->out.link(manipOutLeft->input);

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    // Output queues will be used to get the grayscale frames
    auto qRight = device.getOutputQueue(manipOutRight->getStreamName(), 4, false);
    auto qLeft = device.getOutputQueue(manipOutLeft->getStreamName(), 4, false);
    auto controlQueue = device.getInputQueue(controlIn->getStreamName());
    auto configQueue = device.getInputQueue(configIn->getStreamName());

    // Defaults and limits for manual focus/exposure controls
    int exp_time = 20000;
    int exp_min = 1;
    int exp_max = 33000;

    int sens_iso = 800;
    int sens_min = 100;
    int sens_max = 1600;

    while(true) {
        auto inRight = qRight->get<dai::ImgFrame>();
        auto inLeft = qLeft->get<dai::ImgFrame>();
        cv::imshow("right", inRight->getCvFrame());
        cv::imshow("left", inLeft->getCvFrame());

        // Update screen (1ms pooling rate)
        int key = cv::waitKey(1);
        if(key == 'q') {
            break;
        } else if(key == 'e') {
            printf("Autoexposure enable\n");
            dai::CameraControl ctrl;
            ctrl.setAutoExposureEnable();
            controlQueue->send(ctrl);
        } else if(key == 'i' || key == 'o' || key == 'k' || key == 'l') {
            if(key == 'i') exp_time -= EXP_STEP;
            if(key == 'o') exp_time += EXP_STEP;
            if(key == 'k') sens_iso -= ISO_STEP;
            if(key == 'l') sens_iso += ISO_STEP;
            exp_time = clamp(exp_time, exp_min, exp_max);
            sens_iso = clamp(sens_iso, sens_min, sens_max);
            printf("Setting manual exposure, time: %d, iso: %d\n", exp_time, sens_iso);
            dai::CameraControl ctrl;
            ctrl.setManualExposure(exp_time, sens_iso);
            controlQueue->send(ctrl);
        } else if(key == 'w') {
            if(topLeft.y - stepSize >= 0) {
                topLeft.y -= stepSize;
                bottomRight.y -= stepSize;
                sendCamConfig = true;
            }
        } else if(key == 'a') {
            if(topLeft.x - stepSize >= 0) {
                topLeft.x -= stepSize;
                bottomRight.x -= stepSize;
                sendCamConfig = true;
            }
        } else if(key == 's') {
            if(bottomRight.y + stepSize <= 1) {
                topLeft.y += stepSize;
                bottomRight.y += stepSize;
                sendCamConfig = true;
            }
        } else if(key == 'd') {
            if(bottomRight.x + stepSize <= 1) {
                topLeft.x += stepSize;
                bottomRight.x += stepSize;
                sendCamConfig = true;
            }
        }

        // Send new config to camera
        if(sendCamConfig) {
            dai::ImageManipConfig cfg;
            cfg.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y);
            configQueue->send(cfg);
            sendCamConfig = false;
        }
    }
    return 0;
}

Got questions?

We’re always happy to help with code or other questions you might have.