RGB Encoding & Mono with MobilenetSSD & Depth¶
This example shows how to configure the depthai video encoder in h.265 format to encode the RGB camera input at Full-HD resolution at 30FPS, and transfers the encoded video over XLINK to the host, saving it to disk as a video file. At the same time, a MobileNetv2SSD network is ran on the frames from right grayscale camera, while the application also displays the depth map produced by both of the grayscale cameras. Note that disparity is used in this case, as it colorizes in a more intuitive way.
Pressing Ctrl+C will stop the recording and then convert it using ffmpeg into an mp4 to make it playable. Note that ffmpeg will need to be installed and runnable for the conversion to mp4 to succeed.
Be careful, this example saves encoded video to your host storage. So if you leave it running, you could fill up your storage on your host.
It’s a combination of RGB Encoding and Mono & MobilenetSSD & Depth.
Similar samples:
Demo¶
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
For additional information, please follow installation guide
This example script requires external file(s) to run. If you are using:
depthai-python, run
python3 examples/install_requirements.py
to download required file(s)dephtai-core, required file(s) will get downloaded automatically when building the example
Source code¶
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100 101 102 103 104 105 106 107 108 109 110 111 112 113 114 115 116 117 118 119 120 121 122 123 124 125 126 127 128 129 130 131 132 133 134 135 136 137 138 139 140 141 142 143 144 145 146 147 148 149 150 151 152 153 154 155 156 157 158 159 160 161 162 163 164 165 166 | #!/usr/bin/env python3 from pathlib import Path import sys import cv2 import depthai as dai import numpy as np # Get argument first nnPath = str((Path(__file__).parent / Path('../models/mobilenet-ssd_openvino_2021.4_6shave.blob')).resolve().absolute()) if len(sys.argv) > 1: nnPath = sys.argv[1] if not Path(nnPath).exists(): import sys raise FileNotFoundError(f'Required file/s not found, please run "{sys.executable} install_requirements.py"') # MobilenetSSD label texts labelMap = ["background", "aeroplane", "bicycle", "bird", "boat", "bottle", "bus", "car", "cat", "chair", "cow", "diningtable", "dog", "horse", "motorbike", "person", "pottedplant", "sheep", "sofa", "train", "tvmonitor"] # Create pipeline pipeline = dai.Pipeline() # Define sources and outputs camRgb = pipeline.create(dai.node.ColorCamera) videoEncoder = pipeline.create(dai.node.VideoEncoder) monoRight = pipeline.create(dai.node.MonoCamera) monoLeft = pipeline.create(dai.node.MonoCamera) depth = pipeline.create(dai.node.StereoDepth) manip = pipeline.create(dai.node.ImageManip) nn = pipeline.create(dai.node.MobileNetDetectionNetwork) videoOut = pipeline.create(dai.node.XLinkOut) xoutRight = pipeline.create(dai.node.XLinkOut) disparityOut = pipeline.create(dai.node.XLinkOut) manipOut = pipeline.create(dai.node.XLinkOut) nnOut = pipeline.create(dai.node.XLinkOut) videoOut.setStreamName('h265') xoutRight.setStreamName('right') disparityOut.setStreamName('disparity') manipOut.setStreamName('manip') nnOut.setStreamName('nn') # Properties camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A) camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P) monoRight.setCamera("right") monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P) monoLeft.setCamera("left") monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P) videoEncoder.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H265_MAIN) depth.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY) depth.setRectifyEdgeFillColor(0) # Black, to better see the cutout nn.setConfidenceThreshold(0.5) nn.setBlobPath(nnPath) nn.setNumInferenceThreads(2) nn.input.setBlocking(False) # The NN model expects BGR input. By default ImageManip output type would be same as input (gray in this case) manip.initialConfig.setFrameType(dai.ImgFrame.Type.BGR888p) manip.initialConfig.setResize(300, 300) # Linking camRgb.video.link(videoEncoder.input) videoEncoder.bitstream.link(videoOut.input) monoRight.out.link(xoutRight.input) monoRight.out.link(depth.right) monoLeft.out.link(depth.left) depth.disparity.link(disparityOut.input) depth.rectifiedRight.link(manip.inputImage) manip.out.link(nn.input) manip.out.link(manipOut.input) nn.out.link(nnOut.input) # Disparity range is used for normalization disparityMultiplier = 255 / depth.initialConfig.getMaxDisparity() # Connect to device and start pipeline with dai.Device(pipeline) as device: queueSize = 8 qRight = device.getOutputQueue("right", queueSize) qDisparity = device.getOutputQueue("disparity", queueSize) qManip = device.getOutputQueue("manip", queueSize) qDet = device.getOutputQueue("nn", queueSize) qRgbEnc = device.getOutputQueue('h265', maxSize=30, blocking=True) frame = None frameManip = None frameDisparity = None detections = [] offsetX = (monoRight.getResolutionWidth() - monoRight.getResolutionHeight()) // 2 color = (255, 0, 0) croppedFrame = np.zeros((monoRight.getResolutionHeight(), monoRight.getResolutionHeight())) def frameNorm(frame, bbox): normVals = np.full(len(bbox), frame.shape[0]) normVals[::2] = frame.shape[1] return (np.clip(np.array(bbox), 0, 1) * normVals).astype(int) videoFile = open('video.h265', 'wb') cv2.namedWindow("right", cv2.WINDOW_NORMAL) cv2.namedWindow("manip", cv2.WINDOW_NORMAL) while True: inRight = qRight.tryGet() inManip = qManip.tryGet() inDet = qDet.tryGet() inDisparity = qDisparity.tryGet() while qRgbEnc.has(): qRgbEnc.get().getData().tofile(videoFile) if inRight is not None: frame = inRight.getCvFrame() if inManip is not None: frameManip = inManip.getCvFrame() if inDisparity is not None: # Apply color map for better visualization frameDisparity = inDisparity.getCvFrame() frameDisparity = (frameDisparity*disparityMultiplier).astype(np.uint8) frameDisparity = cv2.applyColorMap(frameDisparity, cv2.COLORMAP_JET) if inDet is not None: detections = inDet.detections if frame is not None: for detection in detections: bbox = frameNorm(croppedFrame, (detection.xmin, detection.ymin, detection.xmax, detection.ymax)) bbox[::2] += offsetX cv2.putText(frame, labelMap[detection.label], (bbox[0] + 10, bbox[1] + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color) cv2.putText(frame, f"{int(detection.confidence * 100)}%", (bbox[0] + 10, bbox[1] + 40), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color) cv2.rectangle(frame, (bbox[0], bbox[1]), (bbox[2], bbox[3]), color, 2) # Show the right cam frame cv2.imshow("right", frame) if frameDisparity is not None: for detection in detections: bbox = frameNorm(croppedFrame, (detection.xmin, detection.ymin, detection.xmax, detection.ymax)) bbox[::2] += offsetX cv2.rectangle(frameDisparity, (bbox[0], bbox[1]), (bbox[2], bbox[3]), color, 2) cv2.putText(frameDisparity, labelMap[detection.label], (bbox[0] + 10, bbox[1] + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color) cv2.putText(frameDisparity, f"{int(detection.confidence * 100)}%", (bbox[0] + 10, bbox[1] + 40), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color) # Show the disparity frame cv2.imshow("disparity", frameDisparity) if frameManip is not None: for detection in detections: bbox = frameNorm(frameManip, (detection.xmin, detection.ymin, detection.xmax, detection.ymax)) cv2.rectangle(frameManip, (bbox[0], bbox[1]), (bbox[2], bbox[3]), color, 2) cv2.putText(frameManip, labelMap[detection.label], (bbox[0] + 10, bbox[1] + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color) cv2.putText(frameManip, f"{int(detection.confidence * 100)}%", (bbox[0] + 10, bbox[1] + 40), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color) # Show the manip frame cv2.imshow("manip", frameManip) if cv2.waitKey(1) == ord('q'): break print("To view the encoded data, convert the stream file (.h265) into a video file (.mp4) using a command below:") print("ffmpeg -framerate 30 -i video.h265 -c copy video.mp4") |
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100 101 102 103 104 105 106 107 108 109 110 111 112 113 114 115 116 117 118 119 120 121 122 123 124 125 126 127 128 129 130 131 132 133 134 135 136 137 138 139 140 141 142 143 144 145 146 147 148 149 150 151 152 153 154 155 156 157 158 159 160 161 162 163 164 165 166 167 168 169 170 171 172 173 174 175 176 177 178 179 180 181 182 183 184 185 186 187 188 189 190 191 192 193 194 195 196 197 198 199 200 201 202 203 204 205 206 207 208 209 | #include <cstdio> #include <iostream> // Includes common necessary includes for development using depthai library #include "depthai/depthai.hpp" // MobilenetSSD label texts static const std::vector<std::string> labelMap = {"background", "aeroplane", "bicycle", "bird", "boat", "bottle", "bus", "car", "cat", "chair", "cow", "diningtable", "dog", "horse", "motorbike", "person", "pottedplant", "sheep", "sofa", "train", "tvmonitor"}; int main(int argc, char** argv) { using namespace std; // Default blob path provided by Hunter private data download // Applicable for easier example usage only std::string nnPath(BLOB_PATH); // If path to blob specified, use that if(argc > 1) { nnPath = std::string(argv[1]); } // Print which blob we are using printf("Using blob at path: %s\n", nnPath.c_str()); // Create pipeline dai::Pipeline pipeline; // Define sources and outputs auto camRgb = pipeline.create<dai::node::ColorCamera>(); auto videoEncoder = pipeline.create<dai::node::VideoEncoder>(); auto monoRight = pipeline.create<dai::node::MonoCamera>(); auto monoLeft = pipeline.create<dai::node::MonoCamera>(); auto depth = pipeline.create<dai::node::StereoDepth>(); auto manip = pipeline.create<dai::node::ImageManip>(); auto nn = pipeline.create<dai::node::MobileNetDetectionNetwork>(); auto videoOut = pipeline.create<dai::node::XLinkOut>(); auto xoutRight = pipeline.create<dai::node::XLinkOut>(); auto disparityOut = pipeline.create<dai::node::XLinkOut>(); auto manipOut = pipeline.create<dai::node::XLinkOut>(); auto nnOut = pipeline.create<dai::node::XLinkOut>(); videoOut->setStreamName("h265"); xoutRight->setStreamName("right"); disparityOut->setStreamName("disparity"); manipOut->setStreamName("manip"); nnOut->setStreamName("nn"); // Properties camRgb->setBoardSocket(dai::CameraBoardSocket::CAM_A); camRgb->setResolution(dai::ColorCameraProperties::SensorResolution::THE_1080_P); monoRight->setCamera("right"); monoRight->setResolution(dai::MonoCameraProperties::SensorResolution::THE_400_P); monoLeft->setCamera("left"); monoLeft->setResolution(dai::MonoCameraProperties::SensorResolution::THE_400_P); videoEncoder->setDefaultProfilePreset(30, dai::VideoEncoderProperties::Profile::H265_MAIN); depth->setDefaultProfilePreset(dai::node::StereoDepth::PresetMode::HIGH_DENSITY); depth->setRectifyEdgeFillColor(0); // Black, to better see the cutout nn->setConfidenceThreshold(0.5); nn->setBlobPath(nnPath); nn->setNumInferenceThreads(2); nn->input.setBlocking(false); // The NN model expects BGR input-> By default ImageManip output type would be same as input (gray in this case) manip->initialConfig.setFrameType(dai::ImgFrame::Type::BGR888p); manip->initialConfig.setResize(300, 300); // Linking camRgb->video.link(videoEncoder->input); videoEncoder->bitstream.link(videoOut->input); monoRight->out.link(xoutRight->input); monoRight->out.link(depth->right); monoLeft->out.link(depth->left); depth->disparity.link(disparityOut->input); depth->rectifiedRight.link(manip->inputImage); manip->out.link(nn->input); manip->out.link(manipOut->input); nn->out.link(nnOut->input); // Disparity range is used for normalization float disparityMultiplier = 255 / depth->initialConfig.getMaxDisparity(); // Connect to device and start pipeline dai::Device device(pipeline); // Queues int queueSize = 8; auto qRight = device.getOutputQueue("right", queueSize); auto qDisparity = device.getOutputQueue("disparity", queueSize); auto qManip = device.getOutputQueue("manip", queueSize); auto qDet = device.getOutputQueue("nn", queueSize); auto qRgbEnc = device.getOutputQueue("h265", 30, true); cv::Mat frame; cv::Mat frameManip; cv::Mat frameDisparity; std::vector<dai::ImgDetection> detections; int offsetX = (monoRight->getResolutionWidth() - monoRight->getResolutionHeight()) / 2; auto color = cv::Scalar(255, 0, 0); auto videoFile = std::ofstream("video.h265", std::ios::binary); cv::namedWindow("right", cv::WINDOW_NORMAL); cv::namedWindow("manip", cv::WINDOW_NORMAL); while(true) { auto inRight = qRight->tryGet<dai::ImgFrame>(); auto inManip = qManip->tryGet<dai::ImgFrame>(); auto inDet = qDet->tryGet<dai::ImgDetections>(); auto inDisparity = qDisparity->tryGet<dai::ImgFrame>(); auto out1 = qRgbEnc->get<dai::ImgFrame>(); videoFile.write((char*)out1->getData().data(), out1->getData().size()); if(inRight) { frame = inRight->getCvFrame(); } if(inManip) { frameManip = inManip->getCvFrame(); } if(inDisparity) { frameDisparity = inDisparity->getCvFrame(); frameDisparity.convertTo(frameDisparity, CV_8UC1, disparityMultiplier); cv::applyColorMap(frameDisparity, frameDisparity, cv::COLORMAP_JET); } if(inDet) { detections = inDet->detections; } if(!frame.empty()) { for(auto& detection : detections) { int x1 = detection.xmin * monoRight->getResolutionHeight() + offsetX; int y1 = detection.ymin * monoRight->getResolutionHeight(); int x2 = detection.xmax * monoRight->getResolutionHeight() + offsetX; int y2 = detection.ymax * monoRight->getResolutionHeight(); uint32_t labelIndex = detection.label; std::string labelStr = to_string(labelIndex); if(labelIndex < labelMap.size()) { labelStr = labelMap[labelIndex]; } cv::putText(frame, labelStr, cv::Point(x1 + 10, y1 + 20), cv::FONT_HERSHEY_TRIPLEX, 0.5, color); std::stringstream confStr; confStr << std::fixed << std::setprecision(2) << detection.confidence * 100; cv::putText(frame, confStr.str(), cv::Point(x1 + 10, y1 + 40), cv::FONT_HERSHEY_TRIPLEX, 0.5, color); cv::rectangle(frame, cv::Rect(cv::Point(x1, y1), cv::Point(x2, y2)), color, cv::FONT_HERSHEY_SIMPLEX); } // Show the right cam frame cv::imshow("right", frame); } if(!frameDisparity.empty()) { for(auto& detection : detections) { int x1 = detection.xmin * monoRight->getResolutionHeight() + offsetX; int y1 = detection.ymin * monoRight->getResolutionHeight(); int x2 = detection.xmax * monoRight->getResolutionHeight() + offsetX; int y2 = detection.ymax * monoRight->getResolutionHeight(); uint32_t labelIndex = detection.label; std::string labelStr = to_string(labelIndex); if(labelIndex < labelMap.size()) { labelStr = labelMap[labelIndex]; } cv::putText(frameDisparity, labelStr, cv::Point(x1 + 10, y1 + 20), cv::FONT_HERSHEY_TRIPLEX, 0.5, color); std::stringstream confStr; confStr << std::fixed << std::setprecision(2) << detection.confidence * 100; cv::putText(frameDisparity, confStr.str(), cv::Point(x1 + 10, y1 + 40), cv::FONT_HERSHEY_TRIPLEX, 0.5, color); cv::rectangle(frameDisparity, cv::Rect(cv::Point(x1, y1), cv::Point(x2, y2)), color, cv::FONT_HERSHEY_SIMPLEX); } // Show the disparity frame cv::imshow("disparity", frameDisparity); } if(!frameManip.empty()) { for(auto& detection : detections) { int x1 = detection.xmin * frameManip.cols; int y1 = detection.ymin * frameManip.rows; int x2 = detection.xmax * frameManip.cols; int y2 = detection.ymax * frameManip.rows; uint32_t labelIndex = detection.label; std::string labelStr = to_string(labelIndex); if(labelIndex < labelMap.size()) { labelStr = labelMap[labelIndex]; } cv::putText(frameManip, labelStr, cv::Point(x1 + 10, y1 + 20), cv::FONT_HERSHEY_TRIPLEX, 0.5, color); std::stringstream confStr; confStr << std::fixed << std::setprecision(2) << detection.confidence * 100; cv::putText(frameManip, confStr.str(), cv::Point(x1 + 10, y1 + 40), cv::FONT_HERSHEY_TRIPLEX, 0.5, color); cv::rectangle(frameManip, cv::Rect(cv::Point(x1, y1), cv::Point(x2, y2)), color, cv::FONT_HERSHEY_SIMPLEX); } // Show the manip frame cv::imshow("manip", frameManip); } int key = cv::waitKey(1); if(key == 'q' || key == 'Q') { break; } } cout << "To view the encoded data, convert the stream file (.h265) into a video file (.mp4), using a command below:" << endl; cout << "ffmpeg -framerate 30 -i video.h265 -c copy video.mp4" << endl; return 0; } |