# Feature Detector

Example shows capabilities of [FeatureTracker](https://docs.luxonis.com/software/depthai/examples/feature_tracker.md). It only
detects features. [Feature Tracker](https://docs.luxonis.com/software/depthai/examples/feature_tracker.md) example also tracks
these features.
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
# Define sources and outputs
monoLeft = pipeline.create(dai.node.MonoCamera)
monoRight = pipeline.create(dai.node.MonoCamera)
featureTrackerLeft = pipeline.create(dai.node.FeatureTracker)
featureTrackerRight = pipeline.create(dai.node.FeatureTracker)

xoutPassthroughFrameLeft = pipeline.create(dai.node.XLinkOut)
xoutTrackedFeaturesLeft = pipeline.create(dai.node.XLinkOut)
xoutPassthroughFrameRight = pipeline.create(dai.node.XLinkOut)
xoutTrackedFeaturesRight = pipeline.create(dai.node.XLinkOut)
xinTrackedFeaturesConfig = pipeline.create(dai.node.XLinkIn)

xoutPassthroughFrameLeft.setStreamName("passthroughFrameLeft")
xoutTrackedFeaturesLeft.setStreamName("trackedFeaturesLeft")
xoutPassthroughFrameRight.setStreamName("passthroughFrameRight")
xoutTrackedFeaturesRight.setStreamName("trackedFeaturesRight")
xinTrackedFeaturesConfig.setStreamName("trackedFeaturesConfig")

# Properties
monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
monoLeft.setCamera("left")
monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
monoRight.setCamera("right")

# Disable optical flow
featureTrackerLeft.initialConfig.setMotionEstimator(False)
featureTrackerRight.initialConfig.setMotionEstimator(False)

# Linking
monoLeft.out.link(featureTrackerLeft.inputImage)
featureTrackerLeft.passthroughInputImage.link(xoutPassthroughFrameLeft.input)
featureTrackerLeft.outputFeatures.link(xoutTrackedFeaturesLeft.input)
xinTrackedFeaturesConfig.out.link(featureTrackerLeft.inputConfig)

monoRight.out.link(featureTrackerRight.inputImage)
featureTrackerRight.passthroughInputImage.link(xoutPassthroughFrameRight.input)
featureTrackerRight.outputFeatures.link(xoutTrackedFeaturesRight.input)
xinTrackedFeaturesConfig.out.link(featureTrackerRight.inputConfig)

featureTrackerConfig = featureTrackerRight.initialConfig.get()

print("Press 's' to switch between Harris and Shi-Thomasi corner detector!")

# Connect to device and start pipeline
with dai.Device(pipeline) as device:

    # Output queues used to receive the results
    passthroughImageLeftQueue = device.getOutputQueue("passthroughFrameLeft", 8, False)
    outputFeaturesLeftQueue = device.getOutputQueue("trackedFeaturesLeft", 8, False)
    passthroughImageRightQueue = device.getOutputQueue("passthroughFrameRight", 8, False)
    outputFeaturesRightQueue = device.getOutputQueue("trackedFeaturesRight", 8, False)

    inputFeatureTrackerConfigQueue = device.getInputQueue("trackedFeaturesConfig")

    leftWindowName = "left"
    rightWindowName = "right"

    def drawFeatures(frame, features):
        pointColor = (0, 0, 255)
        circleRadius = 2
        for feature in features:
            cv2.circle(frame, (int(feature.position.x), int(feature.position.y)), circleRadius, pointColor, -1, cv2.LINE_AA, 0)

    while True:
        inPassthroughFrameLeft = passthroughImageLeftQueue.get()
        passthroughFrameLeft = inPassthroughFrameLeft.getFrame()
        leftFrame = cv2.cvtColor(passthroughFrameLeft, cv2.COLOR_GRAY2BGR)

        inPassthroughFrameRight = passthroughImageRightQueue.get()
        passthroughFrameRight = inPassthroughFrameRight.getFrame()
        rightFrame = cv2.cvtColor(passthroughFrameRight, cv2.COLOR_GRAY2BGR)

        trackedFeaturesLeft = outputFeaturesLeftQueue.get().trackedFeatures
        drawFeatures(leftFrame, trackedFeaturesLeft)

        trackedFeaturesRight = outputFeaturesRightQueue.get().trackedFeatures
        drawFeatures(rightFrame, trackedFeaturesRight)

        # Show the frame
        cv2.imshow(leftWindowName, leftFrame)
        cv2.imshow(rightWindowName, rightFrame)

        key = cv2.waitKey(1)
        if key == ord('q'):
            break
        elif key == ord('s'):
            if featureTrackerConfig.cornerDetector.type == dai.FeatureTrackerConfig.CornerDetector.Type.HARRIS:
                featureTrackerConfig.cornerDetector.type = dai.FeatureTrackerConfig.CornerDetector.Type.SHI_THOMASI
                print("Switching to Shi-Thomasi")
            else:
                featureTrackerConfig.cornerDetector.type = dai.FeatureTrackerConfig.CornerDetector.Type.HARRIS
                print("Switching to Harris")

            cfg = dai.FeatureTrackerConfig()
            cfg.set(featureTrackerConfig)
            inputFeatureTrackerConfigQueue.send(cfg)
```

#### C++

```cpp
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"
#include "deque"
#include "unordered_map"
#include "unordered_set"

static void drawFeatures(cv::Mat& frame, std::vector<dai::TrackedFeature>& features) {
    static const auto pointColor = cv::Scalar(0, 0, 255);
    static const int circleRadius = 2;
    for(auto& feature : features) {
        cv::circle(frame, cv::Point(feature.position.x, feature.position.y), circleRadius, pointColor, -1, cv::LINE_AA, 0);
    }
}

int main() {
    using namespace std;

    // Create pipeline
    dai::Pipeline pipeline;

    // Define sources and outputs
    auto monoLeft = pipeline.create<dai::node::MonoCamera>();
    auto monoRight = pipeline.create<dai::node::MonoCamera>();
    auto featureTrackerLeft = pipeline.create<dai::node::FeatureTracker>();
    auto featureTrackerRight = pipeline.create<dai::node::FeatureTracker>();

    auto xoutPassthroughFrameLeft = pipeline.create<dai::node::XLinkOut>();
    auto xoutTrackedFeaturesLeft = pipeline.create<dai::node::XLinkOut>();
    auto xoutPassthroughFrameRight = pipeline.create<dai::node::XLinkOut>();
    auto xoutTrackedFeaturesRight = pipeline.create<dai::node::XLinkOut>();
    auto xinTrackedFeaturesConfig = pipeline.create<dai::node::XLinkIn>();

    xoutPassthroughFrameLeft->setStreamName("passthroughFrameLeft");
    xoutTrackedFeaturesLeft->setStreamName("trackedFeaturesLeft");
    xoutPassthroughFrameRight->setStreamName("passthroughFrameRight");
    xoutTrackedFeaturesRight->setStreamName("trackedFeaturesRight");
    xinTrackedFeaturesConfig->setStreamName("trackedFeaturesConfig");

    // Properties
    monoLeft->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
    monoLeft->setCamera("left");
    monoRight->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
    monoRight->setCamera("right");

    // Disable optical flow
    featureTrackerLeft->initialConfig.setMotionEstimator(false);
    featureTrackerRight->initialConfig.setMotionEstimator(false);

    // Linking
    monoLeft->out.link(featureTrackerLeft->inputImage);
    featureTrackerLeft->passthroughInputImage.link(xoutPassthroughFrameLeft->input);
    featureTrackerLeft->outputFeatures.link(xoutTrackedFeaturesLeft->input);
    xinTrackedFeaturesConfig->out.link(featureTrackerLeft->inputConfig);

    monoRight->out.link(featureTrackerRight->inputImage);
    featureTrackerRight->passthroughInputImage.link(xoutPassthroughFrameRight->input);
    featureTrackerRight->outputFeatures.link(xoutTrackedFeaturesRight->input);
    xinTrackedFeaturesConfig->out.link(featureTrackerRight->inputConfig);

    auto featureTrackerConfig = featureTrackerRight->initialConfig.get();

    printf("Press 's' to switch between Harris and Shi-Thomasi corner detector! \n");

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    // Output queues used to receive the results
    auto passthroughImageLeftQueue = device.getOutputQueue("passthroughFrameLeft", 8, false);
    auto outputFeaturesLeftQueue = device.getOutputQueue("trackedFeaturesLeft", 8, false);
    auto passthroughImageRightQueue = device.getOutputQueue("passthroughFrameRight", 8, false);
    auto outputFeaturesRightQueue = device.getOutputQueue("trackedFeaturesRight", 8, false);

    auto inputFeatureTrackerConfigQueue = device.getInputQueue("trackedFeaturesConfig");

    const auto leftWindowName = "left";
    const auto rightWindowName = "right";

    while(true) {
        auto inPassthroughFrameLeft = passthroughImageLeftQueue->get<dai::ImgFrame>();
        cv::Mat passthroughFrameLeft = inPassthroughFrameLeft->getFrame();
        cv::Mat leftFrame;
        cv::cvtColor(passthroughFrameLeft, leftFrame, cv::COLOR_GRAY2BGR);

        auto inPassthroughFrameRight = passthroughImageRightQueue->get<dai::ImgFrame>();
        cv::Mat passthroughFrameRight = inPassthroughFrameRight->getFrame();
        cv::Mat rightFrame;
        cv::cvtColor(passthroughFrameRight, rightFrame, cv::COLOR_GRAY2BGR);

        auto trackedFeaturesLeft = outputFeaturesLeftQueue->get<dai::TrackedFeatures>()->trackedFeatures;
        drawFeatures(leftFrame, trackedFeaturesLeft);

        auto trackedFeaturesRight = outputFeaturesRightQueue->get<dai::TrackedFeatures>()->trackedFeatures;
        drawFeatures(rightFrame, trackedFeaturesRight);

        // Show the frame
        cv::imshow(leftWindowName, leftFrame);
        cv::imshow(rightWindowName, rightFrame);

        int key = cv::waitKey(1);
        if(key == 'q') {
            break;
        } else if(key == 's') {
            if(featureTrackerConfig.cornerDetector.type == dai::FeatureTrackerConfig::CornerDetector::Type::HARRIS) {
                featureTrackerConfig.cornerDetector.type = dai::FeatureTrackerConfig::CornerDetector::Type::SHI_THOMASI;
                printf("Switching to Shi-Thomasi \n");
            } else {
                featureTrackerConfig.cornerDetector.type = dai::FeatureTrackerConfig::CornerDetector::Type::HARRIS;
                printf("Switching to Harris \n");
            }
            auto cfg = dai::FeatureTrackerConfig();
            cfg.set(featureTrackerConfig);
            inputFeatureTrackerConfigQueue->send(cfg);
        }
    }
    return 0;
}
```

## Pipeline

Pipeline nodes:
- MonoCamera(0)
- FeatureTracker (2)
- XLinkOut (4)
- XLinkOut (5)
- MonoCamera(1)
- FeatureTracker (3)
- XLinkOut (6)
- XLinkOut (7)
- XLinkIn(8)

Pipeline connections:
- MonoCamera(0) -> FeatureTracker (2) (out -> inputImage)
- XLinkIn(8) -> FeatureTracker (2) (out -> inputConfig)
- FeatureTracker (2) -> XLinkOut (4) (passthroughInputImage -> in)
- FeatureTracker (2) -> XLinkOut (5) (outputFeatures -> in)
- MonoCamera(1) -> FeatureTracker (3) (out -> inputImage)
- XLinkIn(8) -> FeatureTracker (3) (out -> inputConfig)
- FeatureTracker (3) -> XLinkOut (6) (passthroughInputImage -> in)
- FeatureTracker (3) -> XLinkOut (7) (outputFeatures -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.