# RGB-Left Align

This example demonstrates how to align depth information from a left camera to an RGB camera. This is particularly useful for
applications where you need to overlay or compare depth and color data. An OpenCV window is created to display the blended image
of the RGB and aligned depth data. Trackbars are provided to adjust the blending ratio and the static depth plane.

## Demo

![RGB-Left Alignment Demo](https://docs.luxonis.com/static/images/software/depthai/examples/image_align.webp)

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai
from datetime import timedelta
import numpy as np

# This is an interactive example that shows how two frame sources without depth information.
FPS = 30.0

RGB_SOCKET = dai.CameraBoardSocket.CAM_A
LEFT_SOCKET = dai.CameraBoardSocket.CAM_B
ALIGN_SOCKET = LEFT_SOCKET

COLOR_RESOLUTION = dai.ColorCameraProperties.SensorResolution.THE_1080_P
LEFT_RIGHT_RESOLUTION = dai.MonoCameraProperties.SensorResolution.THE_720_P

ISP_SCALE = 3

device = dai.Device()

calibrationHandler = device.readCalibration()
rgbDistortion = calibrationHandler.getDistortionCoefficients(RGB_SOCKET)
distortionModel = calibrationHandler.getDistortionModel(RGB_SOCKET)
if distortionModel != dai.CameraModel.Perspective:
    raise RuntimeError("Unsupported distortion model for RGB camera. This example supports only Perspective model.")

pipeline = dai.Pipeline()

# Define sources and outputs
camRgb = pipeline.create(dai.node.ColorCamera)
left = pipeline.create(dai.node.MonoCamera)
sync = pipeline.create(dai.node.Sync)
out = pipeline.create(dai.node.XLinkOut)
align = pipeline.create(dai.node.ImageAlign)
cfgIn = pipeline.create(dai.node.XLinkIn)

left.setResolution(LEFT_RIGHT_RESOLUTION)
left.setBoardSocket(LEFT_SOCKET)
left.setFps(FPS)

camRgb.setBoardSocket(RGB_SOCKET)
camRgb.setResolution(COLOR_RESOLUTION)
camRgb.setFps(FPS)
camRgb.setIspScale(1, ISP_SCALE)

out.setStreamName("out")

sync.setSyncThreshold(timedelta(seconds=0.5 / FPS))

cfgIn.setStreamName("config")

cfg = align.initialConfig.get()
staticDepthPlane = cfg.staticDepthPlane

# Linking
align.outputAligned.link(sync.inputs["aligned"])
camRgb.isp.link(sync.inputs["rgb"])
camRgb.isp.link(align.inputAlignTo)
left.out.link(align.input)
sync.out.link(out.input)
cfgIn.out.link(align.inputConfig)

rgbWeight = 0.4
leftWeight = 0.6

def updateBlendWeights(percentRgb):
    """
    Update the rgb and left weights used to blend rgb/left image

    @param[in] percent_rgb The rgb weight expressed as a percentage (0..100)
    """
    global leftWeight
    global rgbWeight
    rgbWeight = float(percentRgb) / 100.0
    leftWeight = 1.0 - rgbWeight

def updateDepthPlane(depth):
    global staticDepthPlane
    staticDepthPlane = depth

# Connect to device and start pipeline
with device:
    device.startPipeline(pipeline)
    queue = device.getOutputQueue("out", 8, False)
    cfgQ = device.getInputQueue("config")

    # Configure windows; trackbar adjusts blending ratio of rgb/depth
    windowName = "rgb-left"

    # Set the window to be resizable and the initial size
    cv2.namedWindow(windowName, cv2.WINDOW_NORMAL)
    cv2.resizeWindow(windowName, 1280, 720)
    cv2.createTrackbar(
        "RGB Weight %",
        windowName,
        int(rgbWeight * 100),
        100,
        updateBlendWeights,
    )
    cv2.createTrackbar(
        "Static Depth Plane [mm]",
        windowName,
        0,
        2000,
        updateDepthPlane,
    )
    while True:
        messageGroup = queue.get()
        assert isinstance(messageGroup, dai.MessageGroup)
        frameRgb = messageGroup["rgb"]
        assert isinstance(frameRgb, dai.ImgFrame)
        leftAligned = messageGroup["aligned"]
        assert isinstance(leftAligned, dai.ImgFrame)

        frameRgbCv = frameRgb.getCvFrame()
        # Colorize the aligned depth
        leftCv = leftAligned.getCvFrame()

        rgbIntrinsics = calibrationHandler.getCameraIntrinsics(RGB_SOCKET, int(frameRgbCv.shape[1]), int(frameRgbCv.shape[0]))

        cvFrameUndistorted = cv2.undistort(
            frameRgbCv,
            np.array(rgbIntrinsics),
            np.array(rgbDistortion),
        )

        if len(leftCv.shape) == 2:
            leftCv = cv2.cvtColor(leftCv, cv2.COLOR_GRAY2BGR)
        if leftCv.shape != cvFrameUndistorted.shape:
            leftCv = cv2.resize(leftCv, (cvFrameUndistorted.shape[1], cvFrameUndistorted.shape[0]))

        blended = cv2.addWeighted(cvFrameUndistorted, rgbWeight, leftCv, leftWeight, 0)
        cv2.imshow(windowName, blended)

        key = cv2.waitKey(1)
        if key == ord("q"):
            break

        cfg.staticDepthPlane = staticDepthPlane
        cfgQ.send(cfg)
```

#### C++

```cpp
#include <chrono>
#include <opencv2/opencv.hpp>
#include <queue>

#include "depthai/depthai.hpp"

constexpr auto FPS = 30.0;

constexpr auto RGB_SOCKET = dai::CameraBoardSocket::CAM_A;
constexpr auto LEFT_SOCKET = dai::CameraBoardSocket::CAM_B;
constexpr auto ALIGN_SOCKET = LEFT_SOCKET;

constexpr auto COLOR_RESOLUTION = dai::ColorCameraProperties::SensorResolution::THE_1080_P;
constexpr auto LEFT_RIGHT_RESOLUTION = dai::MonoCameraProperties::SensorResolution::THE_720_P;

class FPSCounter {
   public:
    void tick() {
        auto now = std::chrono::steady_clock::now();
        frameTimes.push(now);
        if(frameTimes.size() > 100) {
            frameTimes.pop();
        }
    }

    double getFps() {
        if(frameTimes.size() <= 1) return 0;
        auto duration = std::chrono::duration_cast<std::chrono::milliseconds>(frameTimes.back() - frameTimes.front()).count();
        return (frameTimes.size() - 1) * 1000.0 / duration;
    }

   private:
    std::queue<std::chrono::steady_clock::time_point> frameTimes;
};

double rgbWeight = 0.4;
double leftWeight = 0.6;
int staticDepthPlane = 0;

void updateBlendWeights(int percentRgb, void*) {
    rgbWeight = static_cast<double>(percentRgb) / 100.0;
    leftWeight = 1.0 - rgbWeight;
}

void updateDepthPlane(int depth, void*) {
    staticDepthPlane = depth;
}

int main() {
    dai::Pipeline pipeline;

    auto camRgb = pipeline.create<dai::node::ColorCamera>();
    auto left = pipeline.create<dai::node::MonoCamera>();
    auto sync = pipeline.create<dai::node::Sync>();
    auto out = pipeline.create<dai::node::XLinkOut>();
    auto align = pipeline.create<dai::node::ImageAlign>();
    auto cfgIn = pipeline.create<dai::node::XLinkIn>();

    left->setResolution(LEFT_RIGHT_RESOLUTION);
    left->setBoardSocket(LEFT_SOCKET);
    left->setFps(FPS);

    camRgb->setBoardSocket(RGB_SOCKET);
    camRgb->setResolution(COLOR_RESOLUTION);
    camRgb->setFps(FPS);
    camRgb->setIspScale(1, 3);

    out->setStreamName("out");

    sync->setSyncThreshold(std::chrono::milliseconds(static_cast<int>((1 / FPS) * 1000.0 * 0.5)));

    cfgIn->setStreamName("config");

    align->outputAligned.link(sync->inputs["aligned"]);
    camRgb->isp.link(sync->inputs["rgb"]);
    camRgb->isp.link(align->inputAlignTo);
    left->out.link(align->input);
    sync->out.link(out->input);
    cfgIn->out.link(align->inputConfig);

    dai::Device device(pipeline);
    auto queue = device.getOutputQueue("out", 8, false);
    auto cfgQ = device.getInputQueue("config");

    FPSCounter fpsCounter;

    std::string windowName = "rgb-left";
    cv::namedWindow(windowName, cv::WINDOW_NORMAL);
    cv::resizeWindow(windowName, 1280, 720);
    cv::createTrackbar("RGB Weight %", windowName, nullptr, 100, updateBlendWeights);
    cv::createTrackbar("Static Depth Plane [mm]", windowName, nullptr, 2000, updateDepthPlane);

    while(true) {
        auto messageGroup = queue->get<dai::MessageGroup>();
        fpsCounter.tick();

        auto frameRgb = messageGroup->get<dai::ImgFrame>("rgb");
        auto leftAligned = messageGroup->get<dai::ImgFrame>("aligned");

        if(frameRgb && leftAligned) {
            auto frameRgbCv = frameRgb->getCvFrame();
            auto leftCv = leftAligned->getCvFrame();

            if(leftCv.channels() == 1) {
                cv::cvtColor(leftCv, leftCv, cv::COLOR_GRAY2BGR);
            }
            if(leftCv.size() != frameRgbCv.size()) {
                cv::resize(leftCv, leftCv, frameRgbCv.size());
            }

            cv::Mat blended;
            cv::addWeighted(frameRgbCv, rgbWeight, leftCv, leftWeight, 0, blended);
            cv::imshow(windowName, blended);
        }

        int key = cv::waitKey(1);
        if(key == 'q' || key == 'Q') {
            break;
        }

        auto cfg = align->initialConfig.get();
        cfg.staticDepthPlane = staticDepthPlane;
        auto alignConfig = std::make_shared<dai::ImageAlignConfig>();
        alignConfig->set(cfg);
        cfgQ->send(alignConfig);
    }

    return 0;
}
```

## Pipeline

Pipeline nodes:
- ColorCamera(0)
- Sync (2)
- XLinkOut (3)
- ImageAlign (4)
- MonoCamera(1)
- XLinkIn(5)

Pipeline connections:
- ImageAlign (4) -> Sync (2) (outputAligned -> aligned)
- ColorCamera(0) -> Sync (2) (isp -> rgb)
- XLinkIn(5) -> ImageAlign (4) (out -> inputConfig)
- ColorCamera(0) -> ImageAlign (4) (isp -> inputAlignTo)
- MonoCamera(1) -> ImageAlign (4) (out -> input)
- Sync (2) -> XLinkOut (3) (out -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.