# Latency measurement

This example shows how to [ImgFrame](https://docs.luxonis.com/software/depthai-components/messages/img_frame.md)'s
`.getTimestamp()` function in combination with `dai.Clock.now()` to measure the latency since image was captured (more accurately
since it was processed by ISP and timestamp was attached to it) until the frame was received on the host computer.

If you would like to learn more about low-latency, see the documentation page
[here](https://docs.luxonis.com/software/depthai/optimizing.md).

## Demo

This example measures latency of `isp` 1080P output (YUV420 encoded frame) from
[ColorCamera](https://docs.luxonis.com/software/depthai-components/nodes/color_camera.md) running at 60FPS. We get about 33ms,
which is what was measured in [optimizing latency](https://docs.luxonis.com/software/depthai/optimizing.md) docs page as well.

```bash
UsbSpeed.SUPER
Latency: 33.49 ms, Average latency: 33.49 ms, Std: 0.00
Latency: 34.92 ms, Average latency: 34.21 ms, Std: 0.71
Latency: 33.23 ms, Average latency: 33.88 ms, Std: 0.74
Latency: 33.70 ms, Average latency: 33.84 ms, Std: 0.65
Latency: 33.94 ms, Average latency: 33.86 ms, Std: 0.58
Latency: 34.18 ms, Average latency: 33.91 ms, Std: 0.54
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
# This might improve reducing the latency on some systems
pipeline.setXLinkChunkSize(0)

# Define source and output
camRgb = pipeline.create(dai.node.ColorCamera)
camRgb.setFps(60)
camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)

xout = pipeline.create(dai.node.XLinkOut)
xout.setStreamName("out")
camRgb.isp.link(xout.input)

# Connect to device and start pipeline
with dai.Device(pipeline) as device:
    print(device.getUsbSpeed())
    q = device.getOutputQueue(name="out")
    diffs = np.array([])
    while True:
        imgFrame = q.get()
        # Latency in miliseconds 
        latencyMs = (dai.Clock.now() - imgFrame.getTimestamp()).total_seconds() * 1000
        diffs = np.append(diffs, latencyMs)
        print('Latency: {:.2f} ms, Average latency: {:.2f} ms, Std: {:.2f}'.format(latencyMs, np.average(diffs), np.std(diffs)))
        
        # Not relevant for this example
        # cv2.imshow('frame', imgFrame.getCvFrame())
```

#### C++

WIP

## Pipeline

Pipeline nodes:
- Camera(0)
- XLinkOut (1)

Pipeline connections:
- Camera(0) -> XLinkOut (1) (1920x1080 NV12 -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.