# POE set IP

This script allows you to set static or dynamic IP, or clear bootloader config on your OAK-POE device.

> **Note**
> Make sure to set mask and gateway correctly! If they are set incorrectly you will soft-brick your device (you won't be able to access it), and will have to [factory reset](https://docs.luxonis.com/hardware/platform/deploy/poe-deployment-guide.md) your OAK PoE.

> **Note**
> We suggest using the [`oakctl rvc2` device manager](https://docs.luxonis.com/software-v3/depthai/depthai-components/bootloader.md), a CLI tool for interfacing with the bootloader and its configurations.

## Demo

Example script output:

```bash
    Found device with name: 192.168.1.136
    -------------------------------------
    "1" to set a static IPv4 address
    "2" to set a dynamic IPv4 address
    "3" to clear the config
    1
    -------------------------------------
    Enter IPv4: 192.168.1.200
    Enter IPv4 Mask: 255.255.255.0
    Enter IPv4 Gateway: 192.168.1.1
    Flashing static IPv4 192.168.1.200, mask 255.255.255.0, gateway 192.168.1.1 to the POE device. Enter 'y' to confirm. y
    Flashing successful.
```

If you run the same example again after 10 seconds, you will see that IP changed to 192.168.1.200:

```bash
    Found device with name: 192.168.1.200
    -------------------------------------
    "1" to set a static IPv4 address
    "2" to set a dynamic IPv4 address
    "3" to clear the config
```

You can also use the device's `default IP address`, which it will revert to if no DHCP server is detected. For more details on how
this works, please refer to the `No DHCP` section in the [Poe Deployment
Guide](https://docs.luxonis.com/hardware/platform/deploy/poe-deployment-guide.md).

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
import depthai as dai

(found, info) = dai.DeviceBootloader.getFirstAvailableDevice()

def check_str(s: str):
    spl = s.split(".")
    if len(spl) != 4:
        raise ValueError(f"Entered value {s} doesn't contain 3 dots. Value has to be in the following format: '255.255.255.255'")
    for num in spl:
        if 255 < int(num):
            raise ValueError("Entered values can't be above 255!")
    return s

if found:
    print(f'Found device with name: {info.name}')
    print('-------------------------------------')
    print('"1" to set a static IPv4 address')
    print('"2" to set a dynamic IPv4 address')
    print('"3" to clear the config')
    key = input('Enter the number: ').strip()
    print('-------------------------------------')
    if int(key) < 1 or 3 < int(key):
        raise ValueError("Entered value should either be '1', '2' or '3'!")

    with dai.DeviceBootloader(info) as bl:
        if key in ['1', '2']:
            ipv4 = check_str(input("Enter IPv4: ").strip())
            mask = check_str(input("Enter IPv4 Mask: ").strip())
            gateway = check_str(input("Enter IPv4 Gateway: ").strip())
            mode = 'static' if key == '1' else 'dynamic'
            val = input(f"Flashing {mode} IPv4 {ipv4}, mask {mask}, gateway {gateway} to the POE device. Enter 'y' to confirm. ").strip()
            if val != 'y':
                raise Exception("Flashing aborted.")

            conf = dai.DeviceBootloader.Config()
            if key == '1': conf.setStaticIPv4(ipv4, mask, gateway)
            elif key == '2': conf.setDynamicIPv4(ipv4, mask, gateway)
            (success, error) = bl.flashConfig(conf)
        elif key == '3':
            (success, error) = bl.flashConfigClear()

        if not success:
            print(f"Flashing failed: {error}")
        else:
            print(f"Flashing successful.")
```

#### C++

```cpp
#include <chrono>
#include <iostream>
#include <string>

#include "depthai/depthai.hpp"
#include "depthai/xlink/XLinkConnection.hpp"

// for string delimiter
std::vector<int> split(std::string s, std::string delimiter) {
    size_t pos_start = 0, pos_end, delim_len = delimiter.length();
    std::string token;
    std::vector<int> res;

    while((pos_end = s.find(delimiter, pos_start)) != std::string::npos) {
        token = s.substr(pos_start, pos_end - pos_start);
        pos_start = pos_end + delim_len;
        res.push_back(stoi(token));
    }
    res.push_back(stoi(s.substr(pos_start)));
    return res;
}

std::string checkStr(std::string str) {
    std::vector<int> v = split(str, ".");
    if(v.size() != 4) {
        std::cout << "Entered value " << str << " doesn't contain 3 dots. Value has to be in the following format: '255.255.255.255'" << std::endl;
        exit(0);
    }
    for(auto i : v) {
        if(i < 0 || 255 < i) {
            std::cout << "Entered values can't be above 255!" << std::endl;
            exit(0);
        }
    }
    return str;
}

int main(int argc, char** argv) {
    bool found = false;
    dai::DeviceInfo info;
    std::tie(found, info) = dai::DeviceBootloader::getFirstAvailableDevice();
    if(!found) {
        std::cout << "No device found to flash. Exiting." << std::endl;
        return -1;
    }

    std::cout << "Found device with name: " << info.getMxId() << std::endl;
    std::cout << "-------------------------------------" << std::endl;
    std::cout << "\"1\" to set a static IPv4 address" << std::endl;
    std::cout << "\"2\" to set a dynamic IPv4 address" << std::endl;
    std::cout << "\"3\" to clear the config" << std::endl;
    auto key = std::cin.get();
    std::cout << "-------------------------------------" << std::endl;

    bool success = false;
    std::string error;
    dai::DeviceBootloader bl(info, true);
    if(key == '1' || key == '2') {
        std::string ip, mask, gateway, in;

        std::cout << "Enter IPv4: ";
        std::cin >> ip;
        checkStr(ip);

        std::cout << "Enter IPv4 Mask: ";
        std::cin >> mask;
        checkStr(mask);

        std::cout << "Enter IPv4 Gateway: ";
        std::cin >> gateway;
        checkStr(gateway);

        std::string mode = "static";
        if(key == '2') mode = "dynamic";
        std::cout << "Flashing " << mode << " IPv4 " << ip << ", mask " << mask << ", gateway " << gateway << " to the POE device. Enter 'y' to confirm. ";
        std::cin >> in;
        if(in != "y") {
            std::cout << "Flashing aborted.";
            return 0;
        }
        auto conf = dai::DeviceBootloader::Config();
        if(key == '1') {
            conf.setStaticIPv4(ip, mask, gateway);
        } else {
            conf.setDynamicIPv4(ip, mask, gateway);
        }

        std::tie(success, error) = bl.flashConfig(conf);
    } else if(key == '3') {
        std::tie(success, error) = bl.flashConfigClear();
    } else {
        std::cout << "Entered value should either be '1', '2' or '3'!";
        return 0;
    }

    if(success) {
        std::cout << "Flashing successful." << std::endl;
    } else {
        std::cout << "Flashing failed: " << error << std::endl;
    }
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.