# RGB Encoding

This example shows how to configure the depthai video encoder in h.265 format to encode the RGB camera input at 8MP/4K/2160p
(3840x2160) at 30FPS (the maximum possible encoding resolultion possible for the encoder, higher frame-rates are possible at lower
resolutions, like 1440p at 60FPS), and transfers the encoded video over XLINK to the host, saving it to disk as a video file.

Pressing Ctrl+C will stop the recording and then convert it using ffmpeg into an mp4 to make it playable. Note that ffmpeg will
need to be installed and runnable for the conversion to mp4 to succeed.

Be careful, this example saves encoded video to your host storage. So if you leave it running, you could fill up your storage on
your host.

### Similar samples:

 * [RGB & Mono Encoding](https://docs.luxonis.com/software/depthai/examples/rgb_mono_encoding.md)
 * [Encoding Max Limit](https://docs.luxonis.com/software/depthai/examples/encoding_max_limit.md)
 * [# RGB Encoding & MobilenetSSD](https://docs.luxonis.com/software/depthai/examples/rgb_encoding_mobilenet.md)
 * [# RGB Encoding & Mono & MobilenetSSD](https://docs.luxonis.com/software/depthai/examples/rgb_encoding_mono_mobilenet.md)
 * [# RGB Encoding & Mono with MobilenetSSD &
   Depth](https://docs.luxonis.com/software/depthai/examples/rgb_encoding_mono_mobilenet_depth.md)

## Demo

[Video: DepthAI Gen2 Code Example - 04 RGB Encoding](https://www.youtube.com/watch?v=k_4t8h_7OWo)

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import depthai as dai

# Create pipeline
pipeline = dai.Pipeline()

# Define sources and output
camRgb = pipeline.create(dai.node.ColorCamera)
videoEnc = pipeline.create(dai.node.VideoEncoder)
xout = pipeline.create(dai.node.XLinkOut)

xout.setStreamName('h265')

# Properties
camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_4_K)
videoEnc.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H265_MAIN)

# Linking
camRgb.video.link(videoEnc.input)
videoEnc.bitstream.link(xout.input)

# Connect to device and start pipeline
with dai.Device(pipeline) as device:

    # Output queue will be used to get the encoded data from the output defined above
    q = device.getOutputQueue(name="h265", maxSize=30, blocking=True)

    # The .h265 file is a raw stream file (not playable yet)
    with open('video.h265', 'wb') as videoFile:
        print("Press Ctrl+C to stop encoding...")
        try:
            while True:
                h265Packet = q.get()  # Blocking call, will wait until a new data has arrived
                h265Packet.getData().tofile(videoFile)  # Appends the packet data to the opened file
        except KeyboardInterrupt:
            # Keyboard interrupt (Ctrl + C) detected
            pass

    print("To view the encoded data, convert the stream file (.h265) into a video file (.mp4) using a command below:")
    print("ffmpeg -framerate 30 -i video.h265 -c copy video.mp4")
```

#### C++

```cpp
#include <csignal>
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

// Keyboard interrupt (Ctrl + C) detected
static std::atomic<bool> alive{true};
static void sigintHandler(int signum) {
    alive = false;
}

int main(int argc, char** argv) {
    using namespace std;
    std::signal(SIGINT, &sigintHandler);

    // Create pipeline
    dai::Pipeline pipeline;

    // Define sources and outputs
    auto camRgb = pipeline.create<dai::node::ColorCamera>();
    auto videoEnc = pipeline.create<dai::node::VideoEncoder>();
    auto xout = pipeline.create<dai::node::XLinkOut>();

    xout->setStreamName("h265");

    // Properties
    camRgb->setBoardSocket(dai::CameraBoardSocket::CAM_A);
    camRgb->setResolution(dai::ColorCameraProperties::SensorResolution::THE_4_K);
    videoEnc->setDefaultProfilePreset(30, dai::VideoEncoderProperties::Profile::H265_MAIN);

    // Linking
    camRgb->video.link(videoEnc->input);
    videoEnc->bitstream.link(xout->input);

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    // Output queue will be used to get the encoded data from the output defined above
    auto q = device.getOutputQueue("h265", 30, true);

    // The .h265 file is a raw stream file (not playable yet)
    auto videoFile = std::ofstream("video.h265", std::ios::binary);
    cout << "Press Ctrl+C to stop encoding..." << endl;

    while(alive) {
        auto h265Packet = q->get<dai::ImgFrame>();
        videoFile.write((char*)(h265Packet->getData().data()), h265Packet->getData().size());
    }

    cout << "To view the encoded data, convert the stream file (.h265) into a video file (.mp4) using a command below:" << endl;
    cout << "ffmpeg -framerate 30 -i video.h265 -c copy video.mp4" << endl;

    return 0;
}
```

## Pipeline

Pipeline nodes:
- ColorCamera(0)
- VideoEncoder (1)
- XLinkOut (2)

Pipeline connections:
- ColorCamera(0) -> VideoEncoder (1) (video -> in)
- VideoEncoder (1) -> XLinkOut (2) (bitstream -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.