# RGB Full Resolution Saver

This example saves full-resolution 3840x2160 `.jpeg` images when `c` key is pressed. It serves as an example of recording high
resolution frames to disk for the purposes of high-resolution ground-truth data.

Note that each frame consumes above 2MB of storage, so "spamming" capture key could fill up your storage.

### Similar samples:

 * [Mono Full Resolution Saver](https://docs.luxonis.com/software/depthai/examples/mono_full_resolution_saver.md)

## Demo

[Video: DepthAI Gen2 Code Example - 06 RGB Full Resolution Saver](https://www.youtube.com/watch?v=DJYzj7jwyY4)

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import time
from pathlib import Path
import cv2
import depthai as dai

# Create pipeline
pipeline = dai.Pipeline()

camRgb = pipeline.create(dai.node.ColorCamera)
camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_4_K)

xoutRgb = pipeline.create(dai.node.XLinkOut)
xoutRgb.setStreamName("rgb")
camRgb.video.link(xoutRgb.input)

xin = pipeline.create(dai.node.XLinkIn)
xin.setStreamName("control")
xin.out.link(camRgb.inputControl)

# Properties
videoEnc = pipeline.create(dai.node.VideoEncoder)
videoEnc.setDefaultProfilePreset(1, dai.VideoEncoderProperties.Profile.MJPEG)
camRgb.still.link(videoEnc.input)

# Linking
xoutStill = pipeline.create(dai.node.XLinkOut)
xoutStill.setStreamName("still")
videoEnc.bitstream.link(xoutStill.input)

# Connect to device and start pipeline
with dai.Device(pipeline) as device:

    # Output queue will be used to get the rgb frames from the output defined above
    qRgb = device.getOutputQueue(name="rgb", maxSize=30, blocking=False)
    qStill = device.getOutputQueue(name="still", maxSize=30, blocking=True)
    qControl = device.getInputQueue(name="control")

    # Make sure the destination path is present before starting to store the examples
    dirName = "rgb_data"
    Path(dirName).mkdir(parents=True, exist_ok=True)

    while True:
        inRgb = qRgb.tryGet()  # Non-blocking call, will return a new data that has arrived or None otherwise
        if inRgb is not None:
            frame = inRgb.getCvFrame()
            # 4k / 4
            frame = cv2.pyrDown(frame)
            frame = cv2.pyrDown(frame)
            cv2.imshow("rgb", frame)

        if qStill.has():
            fName = f"{dirName}/{int(time.time() * 1000)}.jpeg"
            with open(fName, "wb") as f:
                f.write(qStill.get().getData())
                print('Image saved to', fName)

        key = cv2.waitKey(1)
        if key == ord('q'):
            break
        elif key == ord('c'):
            ctrl = dai.CameraControl()
            ctrl.setCaptureStill(True)
            qControl.send(ctrl)
            print("Sent 'still' event to the camera!")
```

#### C++

```cpp
#include <chrono>
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"
#include "utility.hpp"

int main() {
    using namespace std::chrono;

    // Create pipeline
    dai::Pipeline pipeline;

    // Define source and outputs
    auto camRgb = pipeline.create<dai::node::ColorCamera>();
    auto videoEnc = pipeline.create<dai::node::VideoEncoder>();
    auto xoutJpeg = pipeline.create<dai::node::XLinkOut>();
    auto xoutRgb = pipeline.create<dai::node::XLinkOut>();

    xoutJpeg->setStreamName("jpeg");
    xoutRgb->setStreamName("rgb");

    // Properties
    camRgb->setBoardSocket(dai::CameraBoardSocket::CAM_A);
    camRgb->setResolution(dai::ColorCameraProperties::SensorResolution::THE_4_K);
    videoEnc->setDefaultProfilePreset(camRgb->getFps(), dai::VideoEncoderProperties::Profile::MJPEG);

    // Linking
    camRgb->video.link(xoutRgb->input);
    camRgb->video.link(videoEnc->input);
    videoEnc->bitstream.link(xoutJpeg->input);

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    // Queues
    auto qRgb = device.getOutputQueue("rgb", 30, false);
    auto qJpeg = device.getOutputQueue("jpeg", 30, true);

    std::string dirName = "rgb_data";
    createDirectory(dirName);

    while(true) {
        auto inRgb = qRgb->tryGet<dai::ImgFrame>();
        if(inRgb != NULL) {
            cv::imshow("rgb", inRgb->getCvFrame());
        }

        auto encFrames = qJpeg->tryGetAll<dai::ImgFrame>();
        for(const auto& encFrame : encFrames) {
            uint64_t time = duration_cast<milliseconds>(system_clock::now().time_since_epoch()).count();
            std::stringstream videoStr;
            videoStr << dirName << "/" << time << ".jpeg";
            auto videoFile = std::ofstream(videoStr.str(), std::ios::binary);
            videoFile.write((char*)encFrame->getData().data(), encFrame->getData().size());
        }

        int key = cv::waitKey(1);
        if(key == 'q' || key == 'Q') {
            return 0;
        }
    }
    return 0;
}
```

## Pipeline

Pipeline nodes:
- XLinkIn(2)
- ColorCamera (0)
- XLinkOut (1)
- VideoEncoder (3)
- XLinkOut (4)

Pipeline connections:
- ColorCamera (0) -> XLinkOut (1) (video -> in)
- XLinkIn(2) -> ColorCamera (0) (out -> inputControl)
- ColorCamera (0) -> VideoEncoder (3) (still -> in)
- VideoEncoder (3) -> XLinkOut (4) (bitstream -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.