# Stereo Depth custom Mesh

This example shows how you can load custom mesh to the device and use it for depth calculation. In this example, mesh files are
generated from camera calibration data, but you can also use your own mesh files.

By default, [StereoDepth](https://docs.luxonis.com/software/depthai-components/nodes/stereo_depth.md) will use the same logic as
inside the `def getMesh()` to calculate mesh files whenever horizontal FOV is larger than 90°. You could also force calculate the
mesh using:

```python
stereo = pipeline.create(dai.node.StereoDepth)
# Enable mesh calculation to correct distortion:
stereo.enableDistortionCorrection(True)
```

StereoDepth node also allows you to load mesh files directly from a file path:

```python
stereo = pipeline.create(dai.node.StereoDepth)
stereo.loadMeshFiles('path/to/left_mesh', 'path/to/right_mesh')
```

## Demo

![https://github.com/luxonis/depthai-python/assets/18037362/f2031bd4-0748-4a06-abb1-b52e9a17134e](https://github.com/luxonis/depthai-python/assets/18037362/f2031bd4-0748-4a06-abb1-b52e9a17134e)

On the image above you can see that the rectified frame isn't as wide FOV as the original one, that's because the distortion
correction is applied (in this case via custom mesh files), so the disparity matching can be performed correctly.

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import numpy as np
import depthai as dai
import argparse

parser = argparse.ArgumentParser()
parser.add_argument("-res", "--resolution", type=str, default="720",
    help="Sets the resolution on mono cameras. Options: 800 | 720 | 400")
parser.add_argument("-md", "--mesh_dir", type=str, default=None,
    help="Output directory for mesh files. If not specified mesh files won't be saved")
parser.add_argument("-lm", "--load_mesh", default=False, action="store_true",
    help="Read camera intrinsics, generate mesh files and load them into the stereo node.")
args = parser.parse_args()

meshDirectory = args.mesh_dir  # Output dir for mesh files
generateMesh = args.load_mesh  # Load mesh files
RES_MAP = {
    '800': {'w': 1280, 'h': 800, 'res': dai.MonoCameraProperties.SensorResolution.THE_800_P },
    '720': {'w': 1280, 'h': 720, 'res': dai.MonoCameraProperties.SensorResolution.THE_720_P },
    '400': {'w': 640, 'h': 400, 'res': dai.MonoCameraProperties.SensorResolution.THE_400_P }
}
if args.resolution not in RES_MAP:
    exit("Unsupported resolution!")

resolution = RES_MAP[args.resolution]

def getMesh(calibData):
    M1 = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_B, resolution['w'], resolution['h']))
    d1 = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_B))
    R1 = np.array(calibData.getStereoLeftRectificationRotation())
    M2 = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_C, resolution['w'], resolution['h']))
    d2 = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_C))
    R2 = np.array(calibData.getStereoRightRectificationRotation())
    mapXL, mapYL = cv2.initUndistortRectifyMap(M1, d1, R1, M2, (resolution['w'], resolution['h']), cv2.CV_32FC1)
    mapXR, mapYR = cv2.initUndistortRectifyMap(M2, d2, R2, M2, (resolution['w'], resolution['h']), cv2.CV_32FC1)

    meshCellSize = 16
    meshLeft = []
    meshRight = []

    for y in range(mapXL.shape[0] + 1):
        if y % meshCellSize == 0:
            rowLeft = []
            rowRight = []
            for x in range(mapXL.shape[1] + 1):
                if x % meshCellSize == 0:
                    if y == mapXL.shape[0] and x == mapXL.shape[1]:
                        rowLeft.append(mapYL[y - 1, x - 1])
                        rowLeft.append(mapXL[y - 1, x - 1])
                        rowRight.append(mapYR[y - 1, x - 1])
                        rowRight.append(mapXR[y - 1, x - 1])
                    elif y == mapXL.shape[0]:
                        rowLeft.append(mapYL[y - 1, x])
                        rowLeft.append(mapXL[y - 1, x])
                        rowRight.append(mapYR[y - 1, x])
                        rowRight.append(mapXR[y - 1, x])
                    elif x == mapXL.shape[1]:
                        rowLeft.append(mapYL[y, x - 1])
                        rowLeft.append(mapXL[y, x - 1])
                        rowRight.append(mapYR[y, x - 1])
                        rowRight.append(mapXR[y, x - 1])
                    else:
                        rowLeft.append(mapYL[y, x])
                        rowLeft.append(mapXL[y, x])
                        rowRight.append(mapYR[y, x])
                        rowRight.append(mapXR[y, x])
            if (mapXL.shape[1] % meshCellSize) % 2 != 0:
                rowLeft.append(0)
                rowLeft.append(0)
                rowRight.append(0)
                rowRight.append(0)

            meshLeft.append(rowLeft)
            meshRight.append(rowRight)

    meshLeft = np.array(meshLeft)
    meshRight = np.array(meshRight)

    return meshLeft, meshRight

def saveMeshFiles(meshLeft, meshRight, outputPath):
    print("Saving mesh to:", outputPath)
    meshLeft.tofile(outputPath + "/left_mesh.calib")
    meshRight.tofile(outputPath + "/right_mesh.calib")

def create_pipeline(device: dai.Device) -> dai.Pipeline:
    calibData = device.readCalibration()
    print("Creating Stereo Depth pipeline")
    pipeline = dai.Pipeline()

    camLeft = pipeline.create(dai.node.MonoCamera)
    camLeft.setBoardSocket(dai.CameraBoardSocket.LEFT)

    camRight = pipeline.create(dai.node.MonoCamera)
    camRight.setBoardSocket(dai.CameraBoardSocket.RIGHT)

    xoutRight = pipeline.create(dai.node.XLinkOut)
    xoutRight.setStreamName("right")
    camRight.out.link(xoutRight.input)

    for monoCam in (camLeft, camRight):  # Common config
        monoCam.setResolution(resolution['res'])
        # monoCam.setFps(20.0)

    stereo = pipeline.create(dai.node.StereoDepth)
    camLeft.out.link(stereo.left)
    camRight.out.link(stereo.right)
    stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
    stereo.setRectifyEdgeFillColor(0)  # Black, to better see the cutout
    stereo.setLeftRightCheck(True)
    stereo.setExtendedDisparity(True)

    

    xoutDisparity = pipeline.create(dai.node.XLinkOut)
    xoutDisparity.setStreamName("disparity")
    stereo.disparity.link(xoutDisparity.input)

    xoutRectifRight = pipeline.create(dai.node.XLinkOut)
    xoutRectifRight.setStreamName("rectifiedRight")
    stereo.rectifiedRight.link(xoutRectifRight.input)

    # Create custom meshes from calibration data. Here you could also
    # load your own mesh files, or generate them in any other way.
    leftMesh, rightMesh = getMesh(calibData)
    if generateMesh:
        meshLeft = list(leftMesh.tobytes())
        meshRight = list(rightMesh.tobytes())
        # Load mesh data to the StereoDepth node
        stereo.loadMeshData(meshLeft, meshRight)

    if meshDirectory is not None:
        saveMeshFiles(leftMesh, rightMesh, meshDirectory)
    return pipeline

with dai.Device() as device:
    device.startPipeline(create_pipeline(device))

    # Create a receive queue for each stream
    qList = [device.getOutputQueue(stream, 8, blocking=False) for stream in ['right', 'rectifiedRight', 'disparity']]

    while True:
        for q in qList:
            name = q.getName()
            frame = q.get().getCvFrame()
            cv2.imshow(name, frame)
        if cv2.waitKey(1) == ord("q"):
            break
```

## Pipeline

Pipeline nodes:
- MonoCamera(0)
- StereoDepth (3)
- XLinkOut (4)
- XLinkOut (5)
- MonoCamera(1)
- XLinkOut (2)

Pipeline connections:
- MonoCamera(1) -> XLinkOut (2) (out -> in)
- MonoCamera(0) -> StereoDepth (3) (out -> left)
- MonoCamera(1) -> StereoDepth (3) (out -> right)
- StereoDepth (3) -> XLinkOut (4) (disparity -> in)
- StereoDepth (3) -> XLinkOut (5) (rectifiedRight -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.