# Stereo Depth Video

This example is an upgraded [Depth Preview](https://docs.luxonis.com/software/depthai/examples/depth_preview.md). It has higher
resolution (720p), each frame can be shown (mono left-right, rectified left-right, disparity and depth). There are 6 modes which
you can select inside the code:

 * `withDepth`: if you turn it off it will became [Mono
   Preview](https://docs.luxonis.com/software/depthai/examples/mono_preview.md), so it will show only the 2 mono cameras
 * `outputDepth`: if you turn it on it will show the depth
 * `lrcheck`: used for better occlusion handling. For more information [click
   here](https://docs.luxonis.com/software/depthai-components/nodes/stereo_depth.md)
 * `extended`: suitable for short range objects. For more information [click
   here](https://docs.luxonis.com/software/depthai-components/nodes/stereo_depth.md)
 * `subpixel`: suitable for long range. For more information [click
   here](https://docs.luxonis.com/software/depthai-components/nodes/stereo_depth.md)

## Stereo Alpha Param

With `--alpha` you can select scaling during the rectification. Values between 0 and 1:

 * 0.0 (default value) means that the rectified images are zoomed and shifted so that only valid pixels are visible (no black
   areas after rectification)
 * 1.0 means that the rectified image is decimated and shifted so that all the pixels from the original images from the cameras
   are retained in the rectified images (no source image pixels are lost).

![https://github.com/luxonis/depthai-python/assets/18037362/887d489a-6bf6-41ac-9b8f-06ab7b0cd488](https://github.com/luxonis/depthai-python/assets/18037362/887d489a-6bf6-41ac-9b8f-06ab7b0cd488)

### Similar samples:

 * [Depth Preview](https://docs.luxonis.com/software/depthai/examples/depth_preview.md)
 * [Stereo Depth from host](https://docs.luxonis.com/software/depthai/examples/stereo_depth_from_host.md)

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import numpy as np
import depthai as dai
import argparse

parser = argparse.ArgumentParser()
parser.add_argument(
    "-res",
    "--resolution",
    type=str,
    default="720",
    help="Sets the resolution on mono cameras. Options: 800 | 720 | 400",
)
parser.add_argument(
    "-md",
    "--mesh_dir",
    type=str,
    default=None,
    help="Output directory for mesh files. If not specified mesh files won't be saved",
)
parser.add_argument(
    "-lm",
    "--load_mesh",
    default=False,
    action="store_true",
    help="Read camera intrinsics, generate mesh files and load them into the stereo node.",
)
parser.add_argument(
    "-rect",
    "--out_rectified",
    default=False,
    action="store_true",
    help="Generate and display rectified streams",
)
parser.add_argument(
    "-lr",
    "--lrcheck",
    default=False,
    action="store_true",
    help="Better handling for occlusions",
)
parser.add_argument(
    "-e",
    "--extended",
    default=False,
    action="store_true",
    help="Closer-in minimum depth, disparity range is doubled",
)
parser.add_argument(
    "-s",
    "--subpixel",
    default=False,
    action="store_true",
    help="Better accuracy for longer distance, fractional disparity 32-levels",
)
parser.add_argument(
    "-m",
    "--median",
    type=str,
    default="7x7",
    help="Choose the size of median filtering. Options: OFF | 3x3 | 5x5 | 7x7 (default)",
)
parser.add_argument(
    "-d",
    "--depth",
    default=False,
    action="store_true",
    help="Display depth frames",
)
parser.add_argument(
    "-swlr",
    "--swap_left_right",
    default=False,
    action="store_true",
    help="Swap left right frames",
)
parser.add_argument(
    "-a",
    "--alpha",
    type=float,
    default=None,
    help="Alpha scaling parameter to increase FOV",
)
args = parser.parse_args()

RES_MAP = {
    '800': {'w': 1280, 'h': 800, 'res': dai.MonoCameraProperties.SensorResolution.THE_800_P },
    '720': {'w': 1280, 'h': 720, 'res': dai.MonoCameraProperties.SensorResolution.THE_720_P },
    '400': {'w': 640, 'h': 400, 'res': dai.MonoCameraProperties.SensorResolution.THE_400_P }
}
if args.resolution not in RES_MAP:
    exit("Unsupported resolution!")

resolution = RES_MAP[args.resolution]

meshDirectory = args.mesh_dir  # Output dir for mesh files
generateMesh = args.load_mesh  # Load mesh files

outRectified = args.out_rectified  # Output and display rectified streams
lrcheck = args.lrcheck  # Better handling for occlusions
extended = args.extended  # Closer-in minimum depth, disparity range is doubled
subpixel = args.subpixel  # Better accuracy for longer distance, fractional disparity 32-levels
depth = args.depth  # Display depth frames

medianMap = {
    "OFF": dai.StereoDepthProperties.MedianFilter.MEDIAN_OFF,
    "3x3": dai.StereoDepthProperties.MedianFilter.KERNEL_3x3,
    "5x5": dai.StereoDepthProperties.MedianFilter.KERNEL_5x5,
    "7x7": dai.StereoDepthProperties.MedianFilter.KERNEL_7x7,
}
if args.median not in medianMap:
    exit("Unsupported median size!")

median = medianMap[args.median]

print("StereoDepth config options:")
print(f"    Resolution:  {resolution['w']}x{resolution['h']}")
print("    Left-Right check:  ", lrcheck)
print("    Extended disparity:", extended)
print("    Subpixel:          ", subpixel)
print("    Median filtering:  ", median)
print("    Generating mesh files:  ", generateMesh)
print("    Outputting mesh files to:  ", meshDirectory)

def getMesh(calibData):
    M1 = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_B, resolution[0], resolution[1]))
    d1 = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_B))
    R1 = np.array(calibData.getStereoLeftRectificationRotation())
    M2 = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_C, resolution[0], resolution[1]))
    d2 = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_C))
    R2 = np.array(calibData.getStereoRightRectificationRotation())
    mapXL, mapYL = cv2.initUndistortRectifyMap(M1, d1, R1, M2, resolution, cv2.CV_32FC1)
    mapXR, mapYR = cv2.initUndistortRectifyMap(M2, d2, R2, M2, resolution, cv2.CV_32FC1)

    meshCellSize = 16
    meshLeft = []
    meshRight = []

    for y in range(mapXL.shape[0] + 1):
        if y % meshCellSize == 0:
            rowLeft = []
            rowRight = []
            for x in range(mapXL.shape[1] + 1):
                if x % meshCellSize == 0:
                    if y == mapXL.shape[0] and x == mapXL.shape[1]:
                        rowLeft.append(mapYL[y - 1, x - 1])
                        rowLeft.append(mapXL[y - 1, x - 1])
                        rowRight.append(mapYR[y - 1, x - 1])
                        rowRight.append(mapXR[y - 1, x - 1])
                    elif y == mapXL.shape[0]:
                        rowLeft.append(mapYL[y - 1, x])
                        rowLeft.append(mapXL[y - 1, x])
                        rowRight.append(mapYR[y - 1, x])
                        rowRight.append(mapXR[y - 1, x])
                    elif x == mapXL.shape[1]:
                        rowLeft.append(mapYL[y, x - 1])
                        rowLeft.append(mapXL[y, x - 1])
                        rowRight.append(mapYR[y, x - 1])
                        rowRight.append(mapXR[y, x - 1])
                    else:
                        rowLeft.append(mapYL[y, x])
                        rowLeft.append(mapXL[y, x])
                        rowRight.append(mapYR[y, x])
                        rowRight.append(mapXR[y, x])
            if (mapXL.shape[1] % meshCellSize) % 2 != 0:
                rowLeft.append(0)
                rowLeft.append(0)
                rowRight.append(0)
                rowRight.append(0)

            meshLeft.append(rowLeft)
            meshRight.append(rowRight)

    meshLeft = np.array(meshLeft)
    meshRight = np.array(meshRight)

    return meshLeft, meshRight

def saveMeshFiles(meshLeft, meshRight, outputPath):
    print("Saving mesh to:", outputPath)
    meshLeft.tofile(outputPath + "/left_mesh.calib")
    meshRight.tofile(outputPath + "/right_mesh.calib")

def getDisparityFrame(frame, cvColorMap):
    maxDisp = stereo.initialConfig.getMaxDisparity()
    disp = (frame * (255.0 / maxDisp)).astype(np.uint8)
    disp = cv2.applyColorMap(disp, cvColorMap)

    return disp

device = dai.Device()
calibData = device.readCalibration()
print("Creating Stereo Depth pipeline")
pipeline = dai.Pipeline()

camLeft = pipeline.create(dai.node.MonoCamera)
camRight = pipeline.create(dai.node.MonoCamera)
stereo = pipeline.create(dai.node.StereoDepth)
xoutLeft = pipeline.create(dai.node.XLinkOut)
xoutRight = pipeline.create(dai.node.XLinkOut)
xoutDisparity = pipeline.create(dai.node.XLinkOut)
xoutDepth = pipeline.create(dai.node.XLinkOut)
xoutRectifLeft = pipeline.create(dai.node.XLinkOut)
xoutRectifRight = pipeline.create(dai.node.XLinkOut)

if args.swap_left_right:
    camLeft.setCamera("right")
    camRight.setCamera("left")
else:
    camLeft.setCamera("left")
    camRight.setCamera("right")

for monoCam in (camLeft, camRight):  # Common config
    monoCam.setResolution(resolution['res'])
    # monoCam.setFps(20.0)

stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
stereo.initialConfig.setMedianFilter(median)  # KERNEL_7x7 default
stereo.setRectifyEdgeFillColor(0)  # Black, to better see the cutout
stereo.setLeftRightCheck(lrcheck)
stereo.setExtendedDisparity(extended)
stereo.setSubpixel(subpixel)
if args.alpha is not None:
    stereo.setAlphaScaling(args.alpha)
    config = stereo.initialConfig.get()
    config.postProcessing.brightnessFilter.minBrightness = 0
    stereo.initialConfig.set(config)

xoutLeft.setStreamName("left")
xoutRight.setStreamName("right")
xoutDisparity.setStreamName("disparity")
xoutDepth.setStreamName("depth")
xoutRectifLeft.setStreamName("rectifiedLeft")
xoutRectifRight.setStreamName("rectifiedRight")

camLeft.out.link(stereo.left)
camRight.out.link(stereo.right)
stereo.syncedLeft.link(xoutLeft.input)
stereo.syncedRight.link(xoutRight.input)
stereo.disparity.link(xoutDisparity.input)
if depth:
    stereo.depth.link(xoutDepth.input)
if outRectified:
    stereo.rectifiedLeft.link(xoutRectifLeft.input)
    stereo.rectifiedRight.link(xoutRectifRight.input)

streams = ["left", "right"]
if outRectified:
    streams.extend(["rectifiedLeft", "rectifiedRight"])
streams.append("disparity")
if depth:
    streams.append("depth")

cvColorMap = cv2.applyColorMap(np.arange(256, dtype=np.uint8), cv2.COLORMAP_JET)
cvColorMap[0] = [0, 0, 0]
print("Creating DepthAI device")
with device:
    device.startPipeline(pipeline)

    # Create a receive queue for each stream
    qList = [device.getOutputQueue(stream, 8, blocking=False) for stream in streams]

    while True:
        for q in qList:
            name = q.getName()
            frame = q.get().getCvFrame()
            if name == "depth":
                frame = frame.astype(np.uint16)
            elif name == "disparity":
                frame = getDisparityFrame(frame, cvColorMap)

            cv2.imshow(name, frame)
        if cv2.waitKey(1) == ord("q"):
            break
```

#### C++

```cpp
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

static std::atomic<bool> withDepth{true};

static std::atomic<bool> outputDepth{false};
static std::atomic<bool> outputRectified{true};
static std::atomic<bool> lrcheck{true};
static std::atomic<bool> extended{false};
static std::atomic<bool> subpixel{false};

int main() {
    using namespace std;

    // Create pipeline
    dai::Pipeline pipeline;

    // Define sources and outputs
    auto monoLeft = pipeline.create<dai::node::MonoCamera>();
    auto monoRight = pipeline.create<dai::node::MonoCamera>();
    auto stereo = withDepth ? pipeline.create<dai::node::StereoDepth>() : nullptr;

    auto xoutLeft = pipeline.create<dai::node::XLinkOut>();
    auto xoutRight = pipeline.create<dai::node::XLinkOut>();
    auto xoutDisp = pipeline.create<dai::node::XLinkOut>();
    auto xoutDepth = pipeline.create<dai::node::XLinkOut>();
    auto xoutRectifL = pipeline.create<dai::node::XLinkOut>();
    auto xoutRectifR = pipeline.create<dai::node::XLinkOut>();

    // XLinkOut
    xoutLeft->setStreamName("left");
    xoutRight->setStreamName("right");
    if(withDepth) {
        xoutDisp->setStreamName("disparity");
        xoutDepth->setStreamName("depth");
        xoutRectifL->setStreamName("rectified_left");
        xoutRectifR->setStreamName("rectified_right");
    }

    // Properties
    monoLeft->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
    monoLeft->setCamera("left");
    monoRight->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
    monoRight->setCamera("right");

    if(withDepth) {
        // StereoDepth
        stereo->setDefaultProfilePreset(dai::node::StereoDepth::PresetMode::HIGH_DENSITY);
        stereo->setRectifyEdgeFillColor(0);  // black, to better see the cutout
        // stereo->setInputResolution(1280, 720);
        stereo->initialConfig.setMedianFilter(dai::MedianFilter::KERNEL_5x5);
        stereo->setLeftRightCheck(lrcheck);
        stereo->setExtendedDisparity(extended);
        stereo->setSubpixel(subpixel);

        // Linking
        monoLeft->out.link(stereo->left);
        monoRight->out.link(stereo->right);

        stereo->syncedLeft.link(xoutLeft->input);
        stereo->syncedRight.link(xoutRight->input);
        stereo->disparity.link(xoutDisp->input);

        if(outputRectified) {
            stereo->rectifiedLeft.link(xoutRectifL->input);
            stereo->rectifiedRight.link(xoutRectifR->input);
        }

        if(outputDepth) {
            stereo->depth.link(xoutDepth->input);
        }

    } else {
        // Link plugins CAM -> XLINK
        monoLeft->out.link(xoutLeft->input);
        monoRight->out.link(xoutRight->input);
    }

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    auto leftQueue = device.getOutputQueue("left", 8, false);
    auto rightQueue = device.getOutputQueue("right", 8, false);
    auto dispQueue = withDepth ? device.getOutputQueue("disparity", 8, false) : nullptr;
    auto depthQueue = withDepth ? device.getOutputQueue("depth", 8, false) : nullptr;
    auto rectifLeftQueue = withDepth ? device.getOutputQueue("rectified_left", 8, false) : nullptr;
    auto rectifRightQueue = withDepth ? device.getOutputQueue("rectified_right", 8, false) : nullptr;

    // Disparity range is used for normalization
    float disparityMultiplier = withDepth ? 255 / stereo->initialConfig.getMaxDisparity() : 0;

    while(true) {
        auto left = leftQueue->get<dai::ImgFrame>();
        cv::imshow("left", left->getFrame());
        auto right = rightQueue->get<dai::ImgFrame>();
        cv::imshow("right", right->getFrame());

        if(withDepth) {
            auto disparity = dispQueue->get<dai::ImgFrame>();
            cv::Mat disp(disparity->getCvFrame());
            disp.convertTo(disp, CV_8UC1, disparityMultiplier);  // Extend disparity range
            cv::imshow("disparity", disp);
            cv::Mat disp_color;
            cv::applyColorMap(disp, disp_color, cv::COLORMAP_JET);
            cv::imshow("disparity_color", disp_color);

            if(outputDepth) {
                auto depth = depthQueue->get<dai::ImgFrame>();
                cv::imshow("depth", depth->getCvFrame());
            }

            if(outputRectified) {
                auto rectifL = rectifLeftQueue->get<dai::ImgFrame>();
                cv::imshow("rectified_left", rectifL->getFrame());

                auto rectifR = rectifRightQueue->get<dai::ImgFrame>();
                cv::imshow("rectified_right", rectifR->getFrame());
            }
        }

        int key = cv::waitKey(1);
        if(key == 'q' || key == 'Q') {
            return 0;
        }
    }
    return 0;
}
```

## Pipeline

Pipeline nodes:
- MonoCamera(0)
- StereoDepth (2)
- XLinkOut (3)
- XLinkOut (4)
- XLinkOut (5)
- MonoCamera(1)

Pipeline connections:
- MonoCamera(0) -> StereoDepth (2) (out -> left)
- MonoCamera(1) -> StereoDepth (2) (out -> right)
- StereoDepth (2) -> XLinkOut (3) (syncedLeft -> in)
- StereoDepth (2) -> XLinkOut (4) (syncedRight -> in)
- StereoDepth (2) -> XLinkOut (5) (disparity -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.