# RGB-ToF Align

This example demonstrates how to align depth information from a ToF (Time-of-Flight) sensor to an RGB camera. This setup is useful
for applications requiring the overlay or comparison of depth and color data. An OpenCV window is created to display the blended
image of the RGB and aligned depth data. Trackbars are provided to adjust the blending ratio.

## Demo

![RGB-ToF Alignment Demo](https://docs.luxonis.com/static/images/software/depthai/examples/tof_align.webp)

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import numpy as np
import cv2
import depthai as dai
import time
from datetime import timedelta

# This example is intended to run unchanged on an OAK-D-SR-PoE camera
FPS = 30.0

RGB_SOCKET = dai.CameraBoardSocket.CAM_C
TOF_SOCKET = dai.CameraBoardSocket.CAM_A
ALIGN_SOCKET = RGB_SOCKET

class FPSCounter:
    def __init__(self):
        self.frameTimes = []

    def tick(self):
        now = time.time()
        self.frameTimes.append(now)
        self.frameTimes = self.frameTimes[-100:]

    def getFps(self):
        if len(self.frameTimes) <= 1:
            return 0
        # Calculate the FPS
        return (len(self.frameTimes) - 1) / (self.frameTimes[-1] - self.frameTimes[0])

ISP_SCALE = 2

device = dai.Device()

calibrationHandler = device.readCalibration()
rgbDistortion = calibrationHandler.getDistortionCoefficients(RGB_SOCKET)
distortionModel = calibrationHandler.getDistortionModel(RGB_SOCKET)
if distortionModel != dai.CameraModel.Perspective:
    raise RuntimeError("Unsupported distortion model for RGB camera. This example supports only Perspective model.")

pipeline = dai.Pipeline()

# Define sources and outputs
camRgb = pipeline.create(dai.node.ColorCamera)
tof = pipeline.create(dai.node.ToF)
camTof = pipeline.create(dai.node.Camera)
sync = pipeline.create(dai.node.Sync)
align = pipeline.create(dai.node.ImageAlign)
out = pipeline.create(dai.node.XLinkOut)

# ToF settings
camTof.setFps(FPS)
camTof.setImageOrientation(dai.CameraImageOrientation.ROTATE_180_DEG)
camTof.setBoardSocket(TOF_SOCKET)

# rgb settings
camRgb.setBoardSocket(RGB_SOCKET)
camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_800_P)
camRgb.setFps(FPS)
camRgb.setIspScale(1, ISP_SCALE)

out.setStreamName("out")

sync.setSyncThreshold(timedelta(seconds=0.5 / FPS))

# Linking
camRgb.isp.link(sync.inputs["rgb"])
camTof.raw.link(tof.input)
tof.depth.link(align.input)
align.outputAligned.link(sync.inputs["depth_aligned"])
sync.inputs["rgb"].setBlocking(False)
camRgb.isp.link(align.inputAlignTo)
sync.out.link(out.input)

def colorizeDepth(frameDepth):
    invalidMask = frameDepth == 0
    # Log the depth, minDepth and maxDepth
    try:
        minDepth = np.percentile(frameDepth[frameDepth != 0], 3)
        maxDepth = np.percentile(frameDepth[frameDepth != 0], 95)
        logDepth = np.log(frameDepth, where=frameDepth != 0)
        logMinDepth = np.log(minDepth)
        logMaxDepth = np.log(maxDepth)
        np.nan_to_num(logDepth, copy=False, nan=logMinDepth)
        # Clip the values to be in the 0-255 range
        logDepth = np.clip(logDepth, logMinDepth, logMaxDepth)

        # Interpolate only valid logDepth values, setting the rest based on the mask
        depthFrameColor = np.interp(logDepth, (logMinDepth, logMaxDepth), (0, 255))
        depthFrameColor = np.nan_to_num(depthFrameColor)
        depthFrameColor = depthFrameColor.astype(np.uint8)
        depthFrameColor = cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_JET)
        # Set invalid depth pixels to black
        depthFrameColor[invalidMask] = 0
    except IndexError:
        # Frame is likely empty
        depthFrameColor = np.zeros((frameDepth.shape[0], frameDepth.shape[1], 3), dtype=np.uint8)
    except Exception as e:
        raise e
    return depthFrameColor

rgbWeight = 0.4
depthWeight = 0.6

def updateBlendWeights(percentRgb):
    """
    Update the rgb and depth weights used to blend depth/rgb image

    @param[in] percent_rgb The rgb weight expressed as a percentage (0..100)
    """
    global depthWeight
    global rgbWeight
    rgbWeight = float(percentRgb) / 100.0
    depthWeight = 1.0 - rgbWeight

# Connect to device and start pipeline
with device:
    device.startPipeline(pipeline)
    queue = device.getOutputQueue("out", 8, False)

    # Configure windows; trackbar adjusts blending ratio of rgb/depth
    rgbDepthWindowName = "rgb-depth"

    cv2.namedWindow(rgbDepthWindowName)
    cv2.createTrackbar(
        "RGB Weight %",
        rgbDepthWindowName,
        int(rgbWeight * 100),
        100,
        updateBlendWeights,
    )
    fpsCounter = FPSCounter()
    while True:
        messageGroup = queue.get()
        fpsCounter.tick()
        assert isinstance(messageGroup, dai.MessageGroup)
        frameRgb = messageGroup["rgb"]
        assert isinstance(frameRgb, dai.ImgFrame)
        frameDepth = messageGroup["depth_aligned"]
        assert isinstance(frameDepth, dai.ImgFrame)

        sizeRgb = frameRgb.getData().size
        sizeDepth = frameDepth.getData().size
        # Blend when both received
        if frameDepth is not None:
            cvFrame = frameRgb.getCvFrame()
            rgbIntrinsics = calibrationHandler.getCameraIntrinsics(RGB_SOCKET, int(cvFrame.shape[1]), int(cvFrame.shape[0]))
            cvFrameUndistorted = cv2.undistort(
                cvFrame,
                np.array(rgbIntrinsics),
                np.array(rgbDistortion),
            )
            # Colorize the aligned depth
            alignedDepthColorized = colorizeDepth(frameDepth.getFrame())
            # Resize depth to match the rgb frame
            cv2.putText(
                alignedDepthColorized,
                f"FPS: {fpsCounter.getFps():.2f}",
                (10, 30),
                cv2.FONT_HERSHEY_SIMPLEX,
                1,
                (255, 255, 255),
                2,
            )
            cv2.imshow("depth", alignedDepthColorized)

            blended = cv2.addWeighted(
                cvFrameUndistorted, rgbWeight, alignedDepthColorized, depthWeight, 0
            )
            cv2.imshow(rgbDepthWindowName, blended)

        key = cv2.waitKey(1)
        if key == ord("q"):
            break
```

#### C++

```cpp
#include <opencv2/opencv.hpp>

#include "depthai/depthai.hpp"

constexpr auto FPS = 30.0;

constexpr auto RGB_SOCKET = dai::CameraBoardSocket::CAM_B;
constexpr auto TOF_SOCKET = dai::CameraBoardSocket::CAM_A;
constexpr auto ALIGN_SOCKET = RGB_SOCKET;

class FPSCounter {
   public:
    void tick() {
        auto now = std::chrono::steady_clock::now();
        frameTimes.push(now);
        if(frameTimes.size() > 100) {
            frameTimes.pop();
        }
    }

    double getFps() {
        if(frameTimes.size() <= 1) return 0;
        auto duration = std::chrono::duration_cast<std::chrono::milliseconds>(frameTimes.back() - frameTimes.front()).count();
        return (frameTimes.size() - 1) * 1000.0 / duration;
    }

   private:
    std::queue<std::chrono::steady_clock::time_point> frameTimes;
};

cv::Mat colorizeDepth(const cv::Mat& frameDepth) {
    cv::Mat invalidMask = (frameDepth == 0);
    cv::Mat depthFrameColor;
    try {
        double minDepth = 0.0;
        double maxDepth = 0.0;
        cv::minMaxIdx(frameDepth, &minDepth, &maxDepth, nullptr, nullptr, ~invalidMask);
        if(minDepth == maxDepth) {
            depthFrameColor = cv::Mat::zeros(frameDepth.size(), CV_8UC3);
            return depthFrameColor;
        }
        cv::Mat logDepth;
        frameDepth.convertTo(logDepth, CV_32F);
        cv::log(logDepth, logDepth);
        logDepth.setTo(log(minDepth), invalidMask);
        cv::normalize(logDepth, logDepth, 0, 255, cv::NORM_MINMAX, CV_8UC1);
        cv::applyColorMap(logDepth, depthFrameColor, cv::COLORMAP_JET);
        depthFrameColor.setTo(cv::Scalar(0, 0, 0), invalidMask);
    } catch(const std::exception& e) {
        depthFrameColor = cv::Mat::zeros(frameDepth.size(), CV_8UC3);
    }
    return depthFrameColor;
}

double rgbWeight = 0.4;
double depthWeight = 0.6;

void updateBlendWeights(int percentRgb, void*) {
    rgbWeight = static_cast<double>(percentRgb) / 100.0;
    depthWeight = 1.0 - rgbWeight;
}

int main() {
    dai::Pipeline pipeline;

    auto camRgb = pipeline.create<dai::node::ColorCamera>();
    auto camTof = pipeline.create<dai::node::Camera>();
    auto tof = pipeline.create<dai::node::ToF>();
    auto sync = pipeline.create<dai::node::Sync>();
    auto align = pipeline.create<dai::node::ImageAlign>();
    auto xout = pipeline.create<dai::node::XLinkOut>();

    camTof->setFps(FPS);
    camTof->setImageOrientation(dai::CameraImageOrientation::ROTATE_180_DEG);
    camTof->setBoardSocket(TOF_SOCKET);

    camRgb->setBoardSocket(RGB_SOCKET);
    camRgb->setResolution(dai::ColorCameraProperties::SensorResolution::THE_800_P);
    camRgb->setFps(FPS);
    camRgb->setIspScale(1, 2);

    xout->setStreamName("out");

    sync->setSyncThreshold(std::chrono::milliseconds(static_cast<int>(1000 / FPS)));

    camRgb->isp.link(sync->inputs["rgb"]);
    camTof->raw.link(tof->input);
    tof->depth.link(align->input);
    align->outputAligned.link(sync->inputs["depth_aligned"]);
    camRgb->isp.link(align->inputAlignTo);
    sync->out.link(xout->input);

    dai::Device device(pipeline);
    auto queue = device.getOutputQueue("out", 8, false);

    FPSCounter fpsCounter;

    std::string rgbDepthWindowName = "rgb-depth";
    cv::namedWindow(rgbDepthWindowName);
    cv::createTrackbar("RGB Weight %", rgbDepthWindowName, nullptr, 100, updateBlendWeights);

    while(true) {
        auto messageGroup = queue->get<dai::MessageGroup>();
        fpsCounter.tick();

        auto frameRgb = messageGroup->get<dai::ImgFrame>("rgb");
        auto frameDepth = messageGroup->get<dai::ImgFrame>("depth_aligned");

        if(frameRgb && frameDepth) {
            auto cvFrame = frameRgb->getCvFrame();
            auto alignedDepthColorized = colorizeDepth(frameDepth->getFrame());

            cv::putText(alignedDepthColorized,
                        "FPS: " + std::to_string(fpsCounter.getFps()),
                        cv::Point(10, 30),
                        cv::FONT_HERSHEY_SIMPLEX,
                        1,
                        cv::Scalar(255, 255, 255),
                        2);

            cv::imshow("depth", alignedDepthColorized);

            cv::Mat blended;
            cv::addWeighted(cvFrame, rgbWeight, alignedDepthColorized, depthWeight, 0, blended);
            cv::imshow(rgbDepthWindowName, blended);
        }

        int key = cv::waitKey(1);
        if(key == 'q' || key == 'Q') {
            break;
        }
    }

    return 0;
}
```

## Pipeline

Pipeline nodes:
- ColorCamera(0)
- Sync (3)
- XLinkOut (5)
- ImageAlign (4)
- Camera(2)
- ToF (1)

Pipeline connections:
- ColorCamera(0) -> Sync (3) (isp -> rgb)
- ImageAlign (4) -> Sync (3) (outputAligned -> depth_aligned)
- Camera(2) -> ToF (1) (raw -> input)
- ToF (1) -> ImageAlign (4) (depth -> input)
- ColorCamera(0) -> ImageAlign (4) (isp -> inputAlignTo)
- Sync (3) -> XLinkOut (5) (out -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.