# ToF Depth

This is a sample code that showcases how to use the ToF sensor. The [ToF
node](https://docs.luxonis.com/software/depthai-components/nodes/tof.md) converts raw data from the ToF sensor into a depth map.

## Demo

This demo was recorded using the [OAK-D ToF](hw-catalog://OAK-D ToF) that's why we selected CAM_A port on the ToF sensor.

[Video: Real-Time ToF Camera Demonstration](https://www.youtube.com/watch?v=BbBalUzze4s)

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

```python
#!/usr/bin/env python3

import time
import cv2
import depthai as dai
import numpy as np

print(dai.__version__)

cvColorMap = cv2.applyColorMap(np.arange(256, dtype=np.uint8), cv2.COLORMAP_JET)
cvColorMap[0] = [0, 0, 0]

def create_pipeline():
    pipeline = dai.Pipeline()

    tof = pipeline.create(dai.node.ToF)

    # Configure the ToF node
    tofConfig = tof.initialConfig.get()

    # Optional. Best accuracy, but adds motion blur.
    # see ToF node docs on how to reduce/eliminate motion blur.
    tofConfig.enableOpticalCorrection = True
    tofConfig.enablePhaseShuffleTemporalFilter = True
    tofConfig.phaseUnwrappingLevel = 4
    tofConfig.phaseUnwrapErrorThreshold = 300

    tofConfig.enableTemperatureCorrection = False # Not yet supported

    xinTofConfig = pipeline.create(dai.node.XLinkIn)
    xinTofConfig.setStreamName("tofConfig")
    xinTofConfig.out.link(tof.inputConfig)

    tof.initialConfig.set(tofConfig)

    cam_tof = pipeline.create(dai.node.Camera)
    cam_tof.setFps(60) # ToF node will produce depth frames at /2 of this rate
    cam_tof.setBoardSocket(dai.CameraBoardSocket.CAM_A)
    cam_tof.raw.link(tof.input)

    xout = pipeline.create(dai.node.XLinkOut)
    xout.setStreamName("depth")
    tof.depth.link(xout.input)

    tofConfig = tof.initialConfig.get()

    return pipeline, tofConfig

if __name__ == '__main__':
    pipeline, tofConfig = create_pipeline()

    with dai.Device(pipeline) as device:
        print('Connected cameras:', device.getConnectedCameraFeatures())
        qDepth = device.getOutputQueue(name="depth")

        tofConfigInQueue = device.getInputQueue("tofConfig")

        counter = 0
        while True:
            start = time.time()
            key = cv2.waitKey(1)
            if key == ord('f'):
                tofConfig.enableFPPNCorrection = not tofConfig.enableFPPNCorrection
                tofConfigInQueue.send(tofConfig)
            elif key == ord('o'):
                tofConfig.enableOpticalCorrection = not tofConfig.enableOpticalCorrection
                tofConfigInQueue.send(tofConfig)
            elif key == ord('w'):
                tofConfig.enableWiggleCorrection = not tofConfig.enableWiggleCorrection
                tofConfigInQueue.send(tofConfig)
            elif key == ord('t'):
                tofConfig.enableTemperatureCorrection = not tofConfig.enableTemperatureCorrection
                tofConfigInQueue.send(tofConfig)
            elif key == ord('q'):
                break
            elif key == ord('0'):
                tofConfig.enablePhaseUnwrapping = False
                tofConfig.phaseUnwrappingLevel = 0
                tofConfigInQueue.send(tofConfig)
            elif key == ord('1'):
                tofConfig.enablePhaseUnwrapping = True
                tofConfig.phaseUnwrappingLevel = 1
                tofConfigInQueue.send(tofConfig)
            elif key == ord('2'):
                tofConfig.enablePhaseUnwrapping = True
                tofConfig.phaseUnwrappingLevel = 2
                tofConfigInQueue.send(tofConfig)
            elif key == ord('3'):
                tofConfig.enablePhaseUnwrapping = True
                tofConfig.phaseUnwrappingLevel = 3
                tofConfigInQueue.send(tofConfig)
            elif key == ord('4'):
                tofConfig.enablePhaseUnwrapping = True
                tofConfig.phaseUnwrappingLevel = 4
                tofConfigInQueue.send(tofConfig)
            elif key == ord('5'):
                tofConfig.enablePhaseUnwrapping = True
                tofConfig.phaseUnwrappingLevel = 5
                tofConfigInQueue.send(tofConfig)
            elif key == ord('m'):
                medianSettings = [dai.MedianFilter.MEDIAN_OFF, dai.MedianFilter.KERNEL_3x3, dai.MedianFilter.KERNEL_5x5,
                                  dai.MedianFilter.KERNEL_7x7]
                currentMedian = tofConfig.median
                nextMedian = medianSettings[(medianSettings.index(currentMedian) + 1) % len(medianSettings)]
                print(f"Changing median to {nextMedian.name} from {currentMedian.name}")
                tofConfig.median = nextMedian
                tofConfigInQueue.send(tofConfig)

            imgFrame = qDepth.get()  # blocking call, will wait until a new data has arrived
            depth_map = imgFrame.getFrame()
            max_depth = (tofConfig.phaseUnwrappingLevel + 1) * 1500 # 100MHz modulation freq.
            depth_colorized = np.interp(depth_map, (0, max_depth), (0, 255)).astype(np.uint8)
            depth_colorized = cv2.applyColorMap(depth_colorized, cvColorMap)

            cv2.imshow("Colorized depth", depth_colorized)
            counter += 1

    device.close()
```

## Pipeline

Pipeline nodes:
- XLinkIn(1)
- ToF (0)
- XLinkOut (3)
- Camera(2)

Pipeline connections:
- XLinkIn(1) -> ToF (0) (out -> inputConfig)
- Camera(2) -> ToF (0) (raw -> input)
- ToF (0) -> XLinkOut (3) (depth -> in)

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.