Script HTTP client
This example can only run on OAK POE devices. You need bootloader on/above version 0.0.15. You can flash bootloader by running
python3 examples/bootloader/flash_bootloader.py.Demo
Command Line
1~/depthai-python/examples/Script$ python3 script_http_client.py
2Sending http GET request...
3200 OK
4Public IP: b'123.123.123.123'Setup
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2import depthai as dai
3
4# Start defining a pipeline
5pipeline = dai.Pipeline()
6
7# Script node
8script = pipeline.create(dai.node.Script)
9script.setProcessor(dai.ProcessorType.LEON_CSS)
10script.setScript("""
11 import http.client
12 import time
13
14 node.warn('Sending http GET request...')
15 h1 = http.client.HTTPConnection('api.ipify.org', 80)
16 h1.request("GET", "/")
17 r1 = h1.getresponse()
18 node.warn(f'{r1.status} {r1.reason}')
19 data1 = r1.read()
20 node.warn(f'Public IP: {data1}')
21
22 node.io['end'].send(Buffer(32))
23""")
24
25xout = pipeline.create(dai.node.XLinkOut)
26xout.setStreamName('end')
27script.outputs['end'].link(xout.input)
28
29# Connect to device with pipeline
30with dai.Device(pipeline) as device:
31 device.getOutputQueue("end").get() # Wait for the "end" msgPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.