如何放置它
Python
Python
1pipeline = dai.Pipeline()
2hostCamera = pipeline.create(dai.node.Camera).build()
3aprilTagNode = pipeline.create(dai.node.AprilTag)
4# 将 1920x1080 输出链接到 AprilTag 输入
5hostCamera.requestOutput((1920, 1080)).link(aprilTagNode.inputImage)
6# 为直通帧创建输出队列
7passthroughOutputQueue = aprilTagNode.passthroughInputImage.createOutputQueue()
8# 为检测到的 AprilTags 创建输出队列
9outQueue = aprilTagNode.out.createOutputQueue()输入和输出
限制
RVC2
在 RVC2 设备上,AprilTag 节点在主机上运行,因此性能将受限于主机 CPU。
功能示例
参考
class
dai::node::AprilTag
variable
std::shared_ptr< AprilTagConfig > initialConfig
Initial config to use when calculating spatial location data.
variable
Input inputConfig
Input AprilTagConfig message with ability to modify parameters in runtime. Default queue is non-blocking with size 4.
variable
Input inputImage
Input message with depth data used to retrieve spatial information about detected object. Default queue is non-blocking with size 4.
variable
variable
Output outConfig
variable
Output passthroughInputImage
Passthrough message on which the calculation was performed. Suitable for when input queue is set to non-blocking behavior.
function
AprilTag()function
AprilTag(std::unique_ptr< Properties > props)function
void setWaitForConfigInput(bool wait)Specify whether or not wait until configuration message arrives to inputConfig Input.
Parameters
- wait: True to wait for configuration message, false otherwise.
function
bool getWaitForConfigInput()function
void setNumThreads(int numThreads)Set number of threads to use for AprilTag detection.
Parameters
- numThreads: Number of threads to use.
function
int getNumThreads()function
void setRunOnHost(bool runOnHost)Specify whether to run on host or device By default, the node will run on device.
function
bool runOnHost()Check if the node is set to run on host
function
void run()function
void buildInternal()inline function
DeviceNodeCRTP()inline function
DeviceNodeCRTP(const std::shared_ptr< Device > & device)inline function
DeviceNodeCRTP(std::unique_ptr< Properties > props)inline function
DeviceNodeCRTP(std::unique_ptr< Properties > props, bool confMode)inline function
DeviceNodeCRTP(const std::shared_ptr< Device > & device, std::unique_ptr< Properties > props, bool confMode)需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。