如何放置它
Python
Python
1with dai.Pipeline() as pipeline:
2 gate = pipeline.create(dai.node.Gate)输入和输出
用法
Python
Python
1with dai.Pipeline(device) as pipeline:
2 camera = pipeline.create(dai.node.Camera).build()
3 cameraOut = camera.requestOutput((640, 400), fps=30)
4
5 gate = pipeline.create(dai.node.Gate)
6 cameraOut.link(gate.input)
7 cameraQueue = gate.output.createOutputQueue()
8 gateControlQueue = gate.inputControl.createInputQueue()
9
10 gateControl = dai.GateControl()
11
12 pipeline.start()
13
14 startTime = time.monotonic()
15 gateOpen = True
16
17 # Open gate every odd second and close every even second
18 while pipeline.isRunning():
19 currentTime = time.monotonic()
20 if (startTime-currentTime) % 2 == 0:
21 if not gateOpen:
22 gateControlQueue.send(dai.GateControl.openGate())
23 openGate = True
24 else:
25 if gateOpen:
26 gateControlQueue.send(dai.GateControl.closeGate())
27 gateOpen = False功能示例
- Gate 示例 - 每隔 n 秒 打开和关闭流门。
参考
class
dai::node::Gate
variable
std::shared_ptr< GateControl > initialConfig
variable
Input input
variable
Output output
variable
Input inputControl
function
Gate(std::unique_ptr< Properties > props)function
Gate()function
void setRunOnHost(bool runOnHost)Specify whether to run on host or device By default, the node will run on device.
function
bool runOnHost()function
void run()inline function
DeviceNodeCRTP()inline function
DeviceNodeCRTP(const std::shared_ptr< Device > & device)inline function
DeviceNodeCRTP(std::unique_ptr< Properties > props)inline function
DeviceNodeCRTP(std::unique_ptr< Properties > props, bool confMode)inline function
DeviceNodeCRTP(const std::shared_ptr< Device > & device, std::unique_ptr< Properties > props, bool confMode)需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。