SystemLogger
Supported on:RVC2
如何放置
Python
Python
1pipeline = dai.Pipeline()
2logger = pipeline.create(dai.node.SystemLogger)输入和输出
用法
Python
Python
1pipeline = dai.Pipeline()
2logger = pipeline.create(dai.node.SystemLogger)
3logger.setRate(1) # 1 Hz
4
5sysLogQueue = logger.out.createOutputQueue()功能示例
参考
class
dai::node::SystemLogger
variable
Output out
Outputs SystemInformation[RVC4] message that carries various system information like memory and CPU usage, temperatures, ... For series 2 devices output SystemInformation message, for series 4 devices output SystemInformationRVC4 message
function
void setRate(float hz)Specify logging rate, at which messages will be sent out
Parameters
- hz: Sending rate in hertz (messages per second)
function
float getRate()Gets logging rate, at which messages will be sent out
function
void buildInternal()inline function
DeviceNodeCRTP()inline function
DeviceNodeCRTP(const std::shared_ptr< Device > & device)inline function
DeviceNodeCRTP(std::unique_ptr< Properties > props)inline function
DeviceNodeCRTP(std::unique_ptr< Properties > props, bool confMode)inline function
DeviceNodeCRTP(const std::shared_ptr< Device > & device, std::unique_ptr< Properties > props, bool confMode)需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。