EdgeDetector
Supported on:RVC2
如何放置
Python
Python
1pipeline = dai.Pipeline()
2edgeDetector = pipeline.create(dai.node.EdgeDetector)输入和输出
用法
Python
Python
1pipeline = dai.Pipeline()
2edgeDetector = pipeline.create(dai.node.EdgeDetector)
3
4sobelHorizontalKernel = [[1, 0, -1], [2, 0, -2], [1, 0, -1]]
5sobelVerticalKernel = [[1, 2, 1], [0, 0, 0], [-1, -2, -1]]
6edgeDetector.initialConfig.setSobelFilterKernels(sobelHorizontalKernel, sobelVerticalKernel)功能示例
参考
class
dai::node::EdgeDetector
variable
std::shared_ptr< EdgeDetectorConfig > initialConfig
Initial config to use for edge detection.
variable
Input inputConfig
Input EdgeDetectorConfig message with ability to modify parameters in runtime. Default queue is non-blocking with size 4.
variable
Input inputImage
Input image on which edge detection is performed. Default queue is non-blocking with size 4.
variable
Output outputImage
Outputs image frame with detected edges
variable
Output passthroughInputImage
Passthrough message on which the calculation was performed.
function
EdgeDetector()function
EdgeDetector(std::unique_ptr< Properties > props)function
void setNumFramesPool(int numFramesPool)Specify number of frames in pool.
Parameters
- numFramesPool: How many frames should the pool have
function
void setMaxOutputFrameSize(int maxFrameSize)Specify maximum size of output image.
Parameters
- maxFrameSize: Maximum frame size in bytes
inline function
DeviceNodeCRTP()inline function
DeviceNodeCRTP(const std::shared_ptr< Device > & device)inline function
DeviceNodeCRTP(std::unique_ptr< Properties > props)inline function
DeviceNodeCRTP(std::unique_ptr< Properties > props, bool confMode)inline function
DeviceNodeCRTP(const std::shared_ptr< Device > & device, std::unique_ptr< Properties > props, bool confMode)需要帮助?
请前往 Discussion Forum 获取技术支 持或提出您可能有的任何其他问题。