PointCloud¶
The PointCloud node enables on-device point cloud generation from depth map.
How to place it¶
pipeline = dai.Pipeline()
pointCloud = pipeline.create(dai.node.PointCloud)
dai::Pipeline pipeline;
auto pointCloud = pipeline.create<dai::node::PointCloud>();
Inputs and Outputs¶
┌─────────────────────┐
│ │
inputConfig │ PointCloud │
──────────────►│ │ outputPointCloud
│ ├────────────────►
inputDepth │ │ passthroughDepth
──────────────►│---------------------├────────────────►
└─────────────────────┘
Message types
inputDepth
- ImgFrameinputConfig
- PointCloudConfigoutputPointCloud
- PointCloudDatapassthroughDepth
- ImgFrame (passthrough input depth map)
Example visualization with Open3D¶
import open3d as o3d
import numpy as np
import depthai as dai
pcd = o3d.geometry.PointCloud()
vis = o3d.visualization.VisualizerWithKeyCallback()
vis.create_window()
with dai.Device(pipeline) as device:
coordinateFrame = o3d.geometry.TriangleMesh.create_coordinate_frame(size=1000, origin=[0,0,0])
vis.add_geometry(coordinateFrame)
while device.isPipelineRunning():
inMessage = q.get()
inColor = inMessage["rgb"]
inPointCloud = inMessage["pcl"]
cvColorFrame = inColor.getCvFrame()
if inPointCloud:
points = inPointCloud.getPoints().astype(np.float64)
pcd.points = o3d.utility.Vector3dVector(points)
colors = (cvRGBFrame.reshape(-1, 3) / 255.0).astype(np.float64)
pcd.colors = o3d.utility.Vector3dVector(colors)
vis.update_geometry(pcd)
vis.poll_events()
vis.update_renderer()
vis.destroy_window()
#include <iostream>
#include <open3d/Open3D.h>
#include <depthai/depthai.hpp>
int main() {
auto viewer = std::make_unique<pcl::visualization::PCLVisualizer>("Cloud Viewer");
viewer->addPointCloud<pcl::PointXYZ>(cloud, "cloud");
dai::Device device(pipeline);
auto q = device.getOutputQueue("out", 8, false);
auto qDepth = device.getOutputQueue("depth", 8, false);
while(true) {
std::cout << "Waiting for data" << std::endl;
auto depthImg = qDepth->get<dai::ImgFrame>();
auto pclMsg = q->get<dai::PointCloudData>();
if(!pclMsg) {
std::cout << "No data" << std::endl;
continue;
}
auto frame = depthImg->getCvFrame();
frame.convertTo(frame, CV_8UC1, 255 / depth->initialConfig.getMaxDisparity());
if(pclMsg->getPoints().empty()) {
std::cout << "Empty point cloud" << std::endl;
continue;
}
pcl::PointCloud<pcl::PointXYZ>::Ptr cloud = pclMsg->getPclData();
viewer->updatePointCloud(cloud, "cloud");
viewer->spinOnce(10);
if(viewer->wasStopped()) {
break;
}
}
Examples using PointCloud¶
Reference¶
-
class
depthai.node.
PointCloud
PointCloud node. Computes point cloud from depth frames.
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.PointCloudProperties
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
property
id
Id of node
-
property
initialConfig
Initial config to use when computing the point cloud.
-
property
inputConfig
Input PointCloudConfig message with ability to modify parameters in runtime. Default queue is non-blocking with size 4.
-
property
inputDepth
Input message with depth data used to create the point cloud. Default queue is non-blocking with size 4.
-
property
outputPointCloud
Outputs PointCloudData message
-
property
passthroughDepth
Passthrough depth from which the point cloud was calculated. Suitable for when input queue is set to non-blocking behavior.
-
setNumFramesPool
(self: depthai.node.PointCloud, arg0: int) → None Specify number of frames in pool.
- Parameter
numFramesPool
: How many frames should the pool have
- Parameter
-
class
-
class
dai::node
::
PointCloud
: public dai::NodeCRTP<Node, PointCloud, PointCloudProperties>¶ PointCloud node. Computes point cloud from depth frames.
Public Functions
-
void
setNumFramesPool
(int numFramesPool)¶ Specify number of frames in pool.
- Parameters
numFramesPool
: How many frames should the pool have
Public Members
-
PointCloudConfig
initialConfig
¶ Initial config to use when computing the point cloud.
-
Input
inputConfig
= {*this, "inputConfig", Input::Type::SReceiver, false, 4, {{DatatypeEnum::PointCloudConfig, false}}}¶ Input PointCloudConfig message with ability to modify parameters in runtime. Default queue is non-blocking with size 4.
-
Input
inputDepth
= {*this, "inputDepth", Input::Type::SReceiver, false, 4, true, {{DatatypeEnum::ImgFrame, false}}}¶ Input message with depth data used to create the point cloud. Default queue is non-blocking with size 4.
-
Output
outputPointCloud
= {*this, "outputPointCloud", Output::Type::MSender, {{DatatypeEnum::PointCloudData, false}}}¶ Outputs PointCloudData message
-
Output
passthroughDepth
= {*this, "passthroughDepth", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Passthrough depth from which the point cloud was calculated. Suitable for when input queue is set to non-blocking behavior.
Public Static Attributes
-
static constexpr const char *
NAME
= "PointCloud"¶
Private Members
-
std::shared_ptr<RawPointCloudConfig>
rawConfig
¶
-
void