Image quality comparison¶
Here’s an image comparison between different image sensors captured from OAK-FFC-3P. For more information, see Improving Image Quality docs.
IMX214 (13MP color sensor), IMX378 (12MP color sensor), IMX582 (48MP color sensor)
Click on the image for the unencoded full-resolution sensor comparison image. Note that these images are about 8x digitally zoomed, and you can find full-resolution uncropped frames here (300 MB). Image specifications: Grocery items are at 4m, 33LUX, sensitivity 100ISO. Images were taken at 200ms,300ms,400ms,500ms exposure and combined with an HDR script (on the host).