NeuralNetwork
.blob 格式才能 与 VPU 兼容。有关如何将神经网络 (NN) 编译为 .blob 的说明,请参见此处。如何放置它
Python
Python
1pipeline = dai.Pipeline()
2nn = pipeline.create(dai.node.NeuralNetwork)输入和输出
Passthrough 机制
用法
Python
Python
1pipeline = dai.Pipeline()
2nn = pipeline.create(dai.node.NeuralNetwork)
3nn.setBlobPath(bbBlobPath)
4cam.out.link(nn.input)
5
6# 通过 XLink 将 NN 发送到主机
7nnXout = pipeline.create(dai.node.XLinkOut)
8nnXout.setStreamName("nn")
9nn.out.link(nnXout.input)
10
11with dai.Device(pipeline) as device:
12 qNn = device.getOutputQueue("nn")
13
14 nnData = qNn.get() # 阻塞式
15
16 # NN 可以输出多个层。打印所有层名称:
17 print(nnData.getAllLayerNames())
18
19 # 以 FP16 格式获取名为 "Layer1_FP16" 的层
20 layer1Data = nnData.getLayerFp16("Layer1_FP16")
21
22 # 您现在可以解码您的 NN 的输出了功能示例
参考
class
depthai.node.NeuralNetwork(depthai.Node)
method
getNumInferenceThreads(self) -> int: intHow many inference threads will be used to run the network Returns: Number of threads, 0, 1 or 2. Zero means AUTO
method
method
setBlobPath(self, path: Path)Load network blob into assets and use once pipeline is started. Throws: Error if file doesn't exist or isn't a valid network blob. Parameter ``path``: Path to network blob
method
setNumInferenceThreads(self, numThreads: typing.SupportsInt)How many threads should the node use to run the network. Parameter ``numThreads``: Number of threads to dedicate to this node
method
setNumNCEPerInferenceThread(self, numNCEPerThread: typing.SupportsInt)How many Neural Compute Engines should a single thread use for inference Parameter ``numNCEPerThread``: Number of NCE per thread
method
setNumPoolFrames(self, numFrames: typing.SupportsInt)Specifies how many frames will be available in the pool Parameter ``numFrames``: How many frames will pool have
property
input
Input message with data to be inferred upon Default queue is blocking with size 5
property
inputs
Inputs mapped to network inputs. Useful for inferring from separate data sources Default input is non-blocking with queue size 1 and waits for messages
property
out
Outputs NNData message that carries inference results
property
passthrough
Passthrough message on which the inference was performed. Suitable for when input queue is set to non-blocking behavior.
property
passthroughs
Passthroughs which correspond to specified input
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。