Camera Control

This example shows how to use DepthAI SDK to control the color camera parameters.

Control:      key[dec/inc]  min..max
exposure time:     I   O      1..33000 [us]
sensitivity iso:   K   L    100..1600

To go back to auto controls:
'E' - autoexposure

Demo

Camera Control Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
Also available on GitHub

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
from depthai_sdk import OakCamera

with OakCamera() as oak:
    color = oak.create_camera('color')
    oak.visualize(color, fps=True, scale=2/3)
    oak.start()

    while oak.running():
        key = oak.poll()
        if key == ord('i'):
            color.control.exposure_time_down()
        elif key == ord('o'):
            color.control.exposure_time_up()
        elif key == ord('k'):
            color.control.sensitivity_down()
        elif key == ord('l'):
            color.control.sensitivity_up()

        elif key == ord('e'): # Switch to auto exposure
            color.control.send_controls({'exposure': {'auto': True}})

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.