People Tracker on Video Replay

This example shows how to run the people tracker pipeline on a video file.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
from depthai_sdk import OakCamera, ResizeMode

with OakCamera(replay="people-tracking-above-02") as oak:
    color = oak.create_camera('color')
    nn = oak.create_nn('person-detection-0200', color)
    nn.config_nn(resize_mode=ResizeMode.LETTERBOX)
    oak.visualize([color, nn], fps=True)  # 1080P -> 720P
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.