Person Record

This example shows how to set up a trigger with a RecordAction to record both color and disparity frames when a condition is met.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
from depthai_sdk.trigger_action.actions.record_action import RecordAction
from depthai_sdk.trigger_action.triggers.detection_trigger import DetectionTrigger

with OakCamera() as oak:
    color = oak.create_camera('color', encode='jpeg')
    stereo = oak.create_stereo('400p')

    nn = oak.create_nn('mobilenet-ssd', color)

    trigger = DetectionTrigger(input=nn, min_detections={'person': 1}, cooldown=30)
    action = RecordAction(inputs=[color, stereo.out.disparity], dir_path='./recordings/',
                          duration_before_trigger=5, duration_after_trigger=10)
    oak.trigger_action(trigger=trigger, action=action)

    oak.visualize(nn)
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.