Face Detection RGB

This example shows how to run face detection on RGB camera input using SDK.

For running the same face detection on mono camera, see Face Detection Mono.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Demo

RGB face detection demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
    color = oak.create_camera('color')
    nn = oak.create_nn('face-detection-retail-0004', color)
    oak.visualize([nn.out.main, nn.out.passthrough], scale=2/3, fps=True)
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.