Object counting on images

This example cycles through a folder of images and counts the number of objects (people in our case) in each image. It displays the count number on the top of the image. It cycles through each image every 3 seconds, but you can change that with:

with OakCamera('path/to/folder') as oak:
  oak.replay.set_fps(0.5) # For switching cycling through image every 2 seconds
  # ...

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Demo

Counter demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
20
21
22
23
24
25
26
27
#!/usr/bin/env python3

import cv2

from depthai_sdk import OakCamera
from depthai_sdk.classes import DetectionPacket
from depthai_sdk.visualize.configs import TextPosition


def callback(packet: DetectionPacket):
    visualizer = packet.visualizer
    num = len(packet.img_detections.detections)
    print('New msgs! Number of people detected:', num)

    visualizer.add_text(f"Number of people: {num}", position=TextPosition.TOP_MID)
    visualizer.draw(packet.frame)
    cv2.imshow(f'frame {packet.name}', packet.frame)


with OakCamera(replay='people-images-01') as oak:
    color = oak.create_camera('color')
    nn = oak.create_nn('person-detection-retail-0013', color)
    oak.replay.set_fps(0.5)

    oak.visualize(nn, callback=callback)
    # oak.show_graph()
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.