Neural Network Component

This example shows how to run run a color camera stream through a YoloV7 model and display the results on the host.

For additional models, check: models supported by SDK

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
    color = oak.create_camera('color')
    # List of models that are supported out-of-the-box by the SDK:
    # https://docs.luxonis.com/projects/sdk/en/latest/features/ai_models/#sdk-supported-models
    nn = oak.create_nn('yolov5n_coco_416x416', color)
    nn.config_nn(resize_mode='stretch')
    oak.visualize([nn.out.main], fps=True)
    oak.visualize(nn.out.passthrough)
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.