Preview All Cameras

This example shows how to set up a pipeline that outputs a a preview for each camera currently connected (and available) to the device. The preview is displayed in a window on the host machine. If run on OAK-D devices, this example does the same thing as the sdk_camera_preview example.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Demo

Camera Preview Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
Also available on GitHub

1
2
3
4
5
6
from depthai_sdk import OakCamera

with OakCamera() as oak:
    cams = oak.create_all_cameras(resolution='max')
    oak.visualize(cams, fps=True)
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.