Face Detection Inference on Downloaded Image

This example shows how to run the face detection neural network model on a downloaded image from a specified url.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Demo

Photo Download Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
with OakCamera(replay='https://images.pexels.com/photos/3184398/pexels-photo-3184398.jpeg?w=800&h=600') as oak:
    color = oak.create_camera('color')
    nn = oak.create_nn('face-detection-retail-0004', color)
    oak.visualize([nn.out.passthrough, nn])
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.