Spatial Detection

This example showcases the usage of spatial detection using MobileNet-SSD neural network.

For more information about spatial configuration (thresholds, averaging), please refer to config spatial reference.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Demo

Spatial Detection Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
Also available on GitHub

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
from depthai_sdk import OakCamera
import depthai as dai

with OakCamera() as oak:
    color = oak.create_camera('color')
    # List of models that are supported out-of-the-box by the SDK:
    # https://docs.luxonis.com/projects/sdk/en/latest/features/ai_models/#sdk-supported-models
    nn = oak.create_nn('yolov6nr3_coco_640x352', color, spatial=True)

    nn.config_spatial(
        bb_scale_factor=0.5, # Scaling bounding box before averaging the depth in that ROI
        lower_threshold=300, # Discard depth points below 30cm
        upper_threshold=10000, # Discard depth pints above 10m
        # Average depth points before calculating X and Y spatial coordinates:
        calc_algo=dai.SpatialLocationCalculatorAlgorithm.AVERAGE
    )

    oak.visualize(nn.out.main, fps=True)
    oak.visualize([nn.out.passthrough, nn.out.spatials])
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.