Preview Encoder

This example shows how to use the callback function to write MJPEG encoded frames from color camera to a file.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
20
21
22
23
from pathlib import Path

from depthai_sdk import OakCamera
from depthai_sdk.recorders.video_writers.av_writer import AvWriter

fourcc = 'h264' # Can be 'mjpeg', 'h264', or 'hevc'

rec = AvWriter(Path('./'), 'color', fourcc=fourcc)

def save_raw_mjpeg(packet):
    rec.write(packet.msg)

with OakCamera() as oak:
    color = oak.create_camera('color', encode=fourcc, fps=20)

    # Stream encoded video packets to host. For visualization, we decode them
    # on the host side, and for callback we write encoded frames directly to disk.
    oak.visualize(color.out.encoded, scale=2 / 3, fps=True)
    oak.callback(color.out.encoded, callback=save_raw_mjpeg)

    oak.start(blocking=True)

rec.close()

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.