Stereo Encoding

This example shows how to encode disparity map and display it using OpenCV.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
import depthai as dai


with OakCamera() as oak:
    stereo = oak.create_stereo('800p', fps=30, encode='h264')

    # Set on-device output colorization, works only for encoded output
    stereo.set_colormap(dai.Colormap.JET)

    oak.visualize(stereo.out.encoded, fps=True)
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.