MCAP IMU Recording

This example showcases how to record IMU data along with depth and save both in an MCAP file.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
from depthai_sdk import OakCamera, RecordType

with OakCamera() as oak:
    left = oak.create_camera('left', resolution='400p', fps=30)
    right = oak.create_camera('right', resolution='400p', fps=30)
    stereo = oak.create_stereo(left=left, right=right)

    imu = oak.create_imu()
    imu.config_imu(report_rate=500, batch_report_threshold=5)

    # Note that for MCAP recording, user has to have ROS installed
    recorder = oak.record([imu, stereo.out.depth], './', RecordType.MCAP)

    oak.visualize([left, stereo])
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.