IMU Rerun Demonstration

This example showcases how to use the integrated IMU sensor on the OAK-D board. In this example, the displaying is done with Rerun (the same core as our DepthAI Viewer).

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Demo

IMU Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script