Stereo Control

This example shows how to change stereo parameter such as confidence threshold, median filter and decimating factor on the fly.

Control:                  key[dec/inc]    min..max
Confidence threshold:          I   O      1....255

Switches:
'K' - Switch median filter
'1' - Switch to decimation factor 1
'2' - Switch to decimation factor 2
'3' - Switch to decimation factor 3

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Demo

Camera Preview Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
20
21
22
23
24
25
26
27
from depthai_sdk import OakCamera

with OakCamera() as oak:
    left = oak.create_camera('left')
    right = oak.create_camera('right')
    stereo = oak.create_stereo(left=left, right=right)
    stereo.config_stereo(lr_check=True)

    oak.visualize([right, stereo.out.disparity], fps=True)
    oak.start()

    while oak.running():
        key = oak.poll()

        if key == ord('i'):
            stereo.control.confidence_threshold_down()
        if key == ord('o'):
            stereo.control.confidence_threshold_up()
        if key == ord('k'):
            stereo.control.switch_median_filter()

        if key == ord('1'):
            stereo.control.send_controls({'postprocessing': {'decimation': {'factor': 1}}})
        if key == ord('2'):
            stereo.control.send_controls({'postprocessing': {'decimation': {'factor': 2}}})
        if key == ord('3'):
            stereo.control.send_controls({'postprocessing': {'decimation': {'factor': 3}}})

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.