ROSBAG Recording

This example showcases the use of SDK to save color, mono, depth and IMU data to a ROSBAG file. This can be useful for recording data for later use, or for testing purposes.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
from depthai_sdk import OakCamera, RecordType

with OakCamera() as oak:
    color = oak.create_camera('color', encode='jpeg', fps=30)
    left = oak.create_camera('left', resolution='800p', encode='jpeg', fps=30)
    right = oak.create_camera('right', resolution='800p', encode='jpeg', fps=30)
    stereo = oak.create_stereo(left=left, right=right)
    stereo.config_stereo(align=color)
    imu = oak.create_imu()
    imu.config_imu(report_rate=400, batch_report_threshold=5)

    # DB3 / ROSBAG. ROSBAG doesn't require having ROS installed, while DB3 does.
    record_components = [left.out.encoded, color.out.encoded, right.out.encoded, stereo.out.depth, imu]
    oak.record(record_components, 'record', record_type=RecordType.ROSBAG)

    # Visualize only color stream
    oak.visualize(color.out.encoded)
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.