Switch Between Models

This example shows how to switch between models on the fly. It uses script node to alter pipeline flow (either to use the yolo model or the mobilenet model).

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
from depthai_sdk import OakCamera
from depthai_sdk.classes.packets import DetectionPacket
import depthai as dai
import cv2

# We use callback, so we only have cv2 window for both models
def cb(packet: DetectionPacket):
    frame = packet.visualizer.draw(packet.frame)
    cv2.imshow('Frame', frame)

with OakCamera() as oak:
    color = oak.create_camera('color')

    script = oak.pipeline.create(dai.node.Script)
    # When Script node receives a message from the host it will switch streaming frames to another NN model
    script.setScript("""
    i = 0
    outputs = ['out1', 'out2']

    while True:
        frame = node.io['frames'].get()

        switch = node.io['switch'].tryGet()
        if switch is not None:
            i += 1
            if len(outputs) <= i:
                i = 0

        node.io[outputs[i]].send(frame)
    """)
    color.stream.link(script.inputs['frames'])

    # We can have multiple models here, not just 2 object detection models
    nn1 = oak.create_nn('yolov6nr3_coco_640x352', input=script.outputs['out1'])
    nn1.config_nn(resize_mode='stretch') # otherwise, BB mappings will be incorrect
    nn2 = oak.create_nn('mobilenet-ssd', input=script.outputs['out2'])
    nn2.config_nn(resize_mode='stretch') # otherwise, BB mappings will be incorrect

    # We will send "switch" message via XLinkIn
    xin = oak.pipeline.create(dai.node.XLinkIn)
    xin.setStreamName('switch')
    xin.out.link(script.inputs['switch'])

    # We don't want syncing, we just want either of the model packets in the callback
    oak.visualize([nn1, nn2], fps=True, callback=cb)

    oak.visualize([nn1.out.passthrough, nn2.out.passthrough], fps=True)

    # oak.show_graph()

    oak.start()
    qin = oak.device.getInputQueue('switch')

    while True:
        key = oak.poll()
        if key == ord('s'):
            print('Switching NN model')
            qin.send(dai.Buffer())
        elif key == ord('q'):
            break

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.