Stereo Preview

This example shows how to display WLS filtered disparity map using OpenCV.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
import cv2

from depthai_sdk import OakCamera
from depthai_sdk.components.stereo_component import WLSLevel
from depthai_sdk.visualize.configs import StereoColor

with OakCamera() as oak:
    stereo = oak.create_stereo('800p', fps=30)

    # Configure postprocessing (done on host)
    stereo.config_postprocessing(colorize=StereoColor.RGBD, colormap=cv2.COLORMAP_MAGMA)
    stereo.config_wls(wls_level=WLSLevel.MEDIUM)  # WLS filtering, use for smoother results

    oak.visualize(stereo.out.depth)
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.