此页面由 AI 自动翻译。查看英文原版

本页目录

  • Reference

EncodedFrame

输出 EncodedFrame 消息,该消息携带编码后的(MJPEG、H264 或 H265)帧数据。此消息的来源是 VideoEncoder 节点。

Reference

class

dai::EncodedFrame

variable
variable
uint32_t instanceNum
variable
unsigned int width
variable
unsigned int height
variable
uint32_t quality
variable
uint32_t bitrate
variable
Profile profile
variable
bool lossless
variable
FrameType type
variable
uint32_t frameOffset
variable
uint32_t frameSize
variable
ImgTransformation transformation
function
~EncodedFrame()
function
unsigned int getInstanceNum()
Retrieves instance number
function
unsigned int getWidth()
Retrieves image width in pixels
function
unsigned int getHeight()
Retrieves image height in pixels
function
std::chrono::microseconds getExposureTime()
Retrieves exposure time
function
int getSensitivity()
Retrieves sensitivity, as an ISO value
function
int getColorTemperature()
Retrieves white-balance color temperature of the light source, in kelvins
function
int getLensPosition()
Retrieves lens position, range 0..255. Returns -1 if not available
function
float getLensPositionRaw()
Retrieves lens position, range 0.0f..1.0f. Returns -1 if not available
function
Fsync getFsync()
Retrieves effective frame sync mode for this frame.
function
int getSensorMode()
Retrieves selected sensor mode index for this frame.
function
float getFps()
Retrieves sensor FPS for this frame.
function
std::optional< float > getSensorTemperature()
Retrieves sensor temperature in degrees Celsius. Returns an empty optional if not available.
function
unsigned int getQuality()
Retrieves the encoding quality
function
unsigned int getBitrate()
Retrieves the encoding bitrate
function
bool getLossless()
Returns true if encoding is lossless (JPEG only)
function
FrameType getFrameType()
Retrieves frame type (H26x only)
function
Profile getProfile()
Retrieves the encoding profile (JPEG, AVC or HEVC)
function
EncodedFrame & setInstanceNum(unsigned int instance)
Instance number relates to the origin of the frame (which camera)
Parameters
  • instance: Instance number
function
EncodedFrame & setWidth(unsigned int width)
Specifies frame width
Parameters
  • width: frame width
function
EncodedFrame & setHeight(unsigned int height)
Specifies frame height
Parameters
  • height: frame height
function
EncodedFrame & setSize(unsigned int width, unsigned int height)
Specifies frame size
Parameters
  • height: frame height
  • width: frame width
function
EncodedFrame & setSize(std::tuple< unsigned int, unsigned int > size)
Specifies frame size
Parameters
  • size: frame size
function
EncodedFrame & setQuality(unsigned int quality)
Specifies the encoding quality
Parameters
  • quality: Encoding quality
function
EncodedFrame & setBitrate(unsigned int bitrate)
Specifies the encoding quality
Parameters
  • quality: Encoding quality
function
EncodedFrame & setLossless(bool lossless)
Specifies if encoding is lossless (JPEG only)
Parameters
  • lossless: True if lossless
function
EncodedFrame & setFrameType(FrameType type)
Specifies the frame type (H26x only)
Parameters
  • type: Type of h26x frame (I, P, B)
function
EncodedFrame & setProfile(Profile profile)
Specifies the encoding profile
Parameters
  • profile: Encoding profile
function
ImgFrame getImgFrameMeta()
function
void serialize(std::vector< std::uint8_t > & metadata, DatatypeEnum & datatype)
inline function
DatatypeEnum getDatatype()
function
DEPTHAI_SERIALIZE(EncodedFrame, cam, instanceNum, width, height, quality, bitrate, profile, lossless, type, frameOffset, frameSize, transformation, Buffer::sequenceNum, Buffer::ts, Buffer::tsDevice)
enum

std::uint8_t Profile

enumerator
JPEG
enumerator
AVC
enumerator
HEVC
enum

std::uint8_t FrameType

enumerator
I
enumerator
P
enumerator
B
enumerator
Unknown
enum

enum

ImgFrame::Fsync Fsync

需要帮助?

请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。