ToFConfig
功能示例
参考
class
dai::ToFConfig
variable
filters::params::MedianFilter median
Set kernel size for depth median filtering, or disable
variable
int phaseUnwrappingLevel
variable
uint16_t phaseUnwrapErrorThreshold
variable
bool enablePhaseShuffleTemporalFilter
variable
bool enableBurstMode
variable
bool enableDistortionCorrection
variable
std::optional< bool > enableFPPNCorrection
variable
std::optional< bool > enableOpticalCorrection
variable
std::optional< bool > enableTemperatureCorrection
variable
std::optional< bool > enableWiggleCorrection
variable
std::optional< bool > enablePhaseUnwrapping
function
ToFConfig()function
~ToFConfig()function
ToFConfig & setMedianFilter(filters::params::MedianFilter median)Parameters
- median: Set kernel size for median filtering, or disable
function
void serialize(std::vector< std::uint8_t > & metadata, DatatypeEnum & datatype)inline function
DatatypeEnum getDatatype()function
void setProfilePreset(ImageFiltersPresetMode presetMode)function
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。