Tracklets
spatialCoordinates(X/Y/Z,单位为 mm)。velocity 和 speed 是可选的 3D 估计值(单位为 m/s),在没有有效空间状态时为空,例如仅 RGB 跟踪。功能示例
参考
class
dai::Tracklets
variable
LengthUnit unit
Measurement unit used by all tracklets'
variable
std::vector< Tracklet > tracklets
variable
int64_t sequenceNum
variable
Timestamp ts
variable
Timestamp tsDevice
variable
std::optional< ImgTransformation > transformation
function
Tracklets()function
~Tracklets()function
Tracklets transformTo(const ImgTransformation & target)Returns a new Tracklets message with the tracklets transformed into the target image transformation.For each tracklet, the bounding box is assumed to lie on a plane parallel to the image plane at depth
Parameters
- target: Target image transformation.
function
void serialize(std::vector< std::uint8_t > & metadata, DatatypeEnum & datatype)function
function
std::optional< ImgTransformation > getTransformation()Returns the current transformation if set, else std::nullopt.
function
void setTransformation(const ImgTransformation & transformation)Sets the current transformation.
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。