EdgeDetectorConfig
功能示例
参考
class
dai::EdgeDetectorConfig
variable
EdgeDetectorConfigData config
function
EdgeDetectorConfig()function
~EdgeDetectorConfig()function
void setSobelFilterKernels(const std::vector< std::vector< int >> & horizontalKernel, const std::vector< std::vector< int >> & verticalKernel)Set sobel filter horizontal and vertical 3x3 kernels
Parameters
- horizontalKernel: Used for horizontal gradient computation in 3x3 Sobel filter
- verticalKernel: Used for vertical gradient computation in 3x3 Sobel filter
function
EdgeDetectorConfigData getConfigData()Retrieve configuration data for EdgeDetector
Returns
EdgeDetectorConfigData: sobel filter horizontal and vertical 3x3 kernels
function
void serialize(std::vector< std::uint8_t > & metadata, DatatypeEnum & datatype)inline function
DatatypeEnum getDatatype()function
DEPTHAI_SERIALIZE(EdgeDetectorConfig, Buffer::sequenceNum, Buffer::ts, Buffer::tsDevice, config)struct
dai::EdgeDetectorConfig::EdgeDetectorConfigData
variable
std::vector< std::vector< int > > sobelFilterHorizontalKernel
Used for horizontal gradient computation in 3x3 Sobel filter Format - 3x3 matrix, 2nd column must be 0 Default - +1 0 -1; +2 0 -2; +1 0 -1
variable
std::vector< std::vector< int > > sobelFilterVerticalKernel
Used for vertical gradient computation in 3x3 Sobel filter Format - 3x3 matrix, 2nd row must be 0 Default - +1 +2 +1; 0 0 0; -1 -2 -1
function
DEPTHAI_SERIALIZE(EdgeDetectorConfigData, sobelFilterHorizontalKernel, sobelFilterVerticalKernel)需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。