IMU 加速度计和陀螺仪
演示
Command Line
1~/examples/IMU$ python3 imu_gyroscope_accelerometer.py
2Accelerometer timestamp: 27 days, 4:31:26.532170
3Latency [ms]: 0:00:00.004806
4Accelerometer [m/s^2]: x: -0.098162 y: -0.062249 z: -9.715671
5Gyroscope timestamp: 27 days, 4:31:26.532170
6Gyroscope [rad/s]: x: 0.002131 y: 0.019175 z: 0.001065
7Accelerometer timestamp: 27 days, 4:31:26.534664
8Latency [ms]: 0:00:00.006309
9Accelerometer [m/s^2]: x: -0.064643 y: -0.119710 z: -9.758766
10Gyroscope timestamp: 27 days, 4:31:26.534664
11Gyroscope [rad/s]: x: 0.002131 y: 0.019175 z: 0.002131设置
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.py源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5import time
6import math
7
8# Create pipeline
9pipeline = dai.Pipeline()
10
11# Define sources and outputs
12imu = pipeline.create(dai.node.IMU)
13xlinkOut = pipeline.create(dai.node.XLinkOut)
14
15xlinkOut.setStreamName("imu")
16
17# enable ACCELEROMETER_RAW at 500 hz rate
18imu.enableIMUSensor(dai.IMUSensor.ACCELEROMETER_RAW, 500)
19# enable GYROSCOPE_RAW at 400 hz rate
20imu.enableIMUSensor(dai.IMUSensor.GYROSCOPE_RAW, 400)
21# it's recommended to set both setBatchReportThreshold and setMaxBatchReports to 20 when integrating in a pipeline with a lot of input/output connections
22# above this threshold packets will be sent in batch of X, if the host is not blocked and USB bandwidth is available
23imu.setBatchReportThreshold(1)
24# maximum number of IMU packets in a batch, if it's reached device will block sending until host can receive it
25# if lower or equal to batchReportThreshold then the sending is always blocking on device
26# useful to reduce device's CPU load and number of lost packets, if CPU load is high on device side due to multiple nodes
27imu.setMaxBatchReports(10)
28
29# Link plugins IMU -> XLINK
30imu.out.link(xlinkOut.input)
31
32# Pipeline is defined, now we can connect to the device
33with dai.Device(pipeline) as device:
34
35 def timeDeltaToMilliS(delta) -> float:
36 return delta.total_seconds()*1000
37
38 # Output queue for imu bulk packets
39 imuQueue = device.getOutputQueue(name="imu", maxSize=50, blocking=False)
40 baseTs = None
41 while True:
42 imuData = imuQueue.get() # blocking call, will wait until a new data has arrived
43
44 imuPackets = imuData.packets
45 for imuPacket in imuPackets:
46 acceleroValues = imuPacket.acceleroMeter
47 gyroValues = imuPacket.gyroscope
48
49 acceleroTs = acceleroValues.getTimestampDevice()
50 gyroTs = gyroValues.getTimestampDevice()
51 if baseTs is None:
52 baseTs = acceleroTs if acceleroTs < gyroTs else gyroTs
53 acceleroTs = timeDeltaToMilliS(acceleroTs - baseTs)
54 gyroTs = timeDeltaToMilliS(gyroTs - baseTs)
55
56 imuF = "{:.06f}"
57 tsF = "{:.03f}"
58
59 print(f"Accelerometer timestamp: {tsF.format(acceleroTs)} ms")
60 print(f"Accelerometer [m/s^2]: x: {imuF.format(acceleroValues.x)} y: {imuF.format(acceleroValues.y)} z: {imuF.format(acceleroValues.z)}")
61 print(f"Gyroscope timestamp: {tsF.format(gyroTs)} ms")
62 print(f"Gyroscope [rad/s]: x: {imuF.format(gyroValues.x)} y: {imuF.format(gyroValues.y)} z: {imuF.format(gyroValues.z)} ")
63
64 if cv2.waitKey(1) == ord('q'):
65 break需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。